QSPI Configuration using SST26VF032B-104I
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-02-19 8:29 PM
Hi STM,
I have some questions for QSPI configuration using SST26VF032B-104I (Max clock = 104 MHz)
I am getting QSPI_SUSPENDED Error when I call BSP_QSPI_GetStatus().
Configuration is as follow;
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
QSPIHandle.Init.ClockPrescaler = 2; /* QSPI freq = 216 MHz/(1+2) = 72 Mhz */
QSPIHandle.Init.FifoThreshold = 4; QSPIHandle.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_HALFCYCLE; QSPIHandle.Init.FlashSize = POSITION_VAL(SST26VF032B_FLASH_SIZE) - 1; QSPIHandle.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_2_CYCLE; /* Min 30ns for nonRead */ QSPIHandle.Init.ClockMode = QSPI_CLOCK_MODE_0; QSPIHandle.Init.FlashID = QSPI_FLASH_ID_1; QSPIHandle.Init.DualFlash = QSPI_DUALFLASH_DISABLE;//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
I don't know what is wrong.
Please advise me.
Thanks.
Regards,
Thiha Kyaw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-02-20 7:27 PM
Hi,
I debugged it and faced the problem.
The error is at Configuring automatic polling mode to wait the QUADEN bit=1 and WIP bit=0 in QSPI_EnterMemory_QPI.
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
/* Configure automatic polling mode to wait the QUADEN bit=1 and WIP bit=0 */
s_config.Match = MX25L512_SR_QUADEN; // Same as SST26VF032B s_config.Mask = MX25L512_SR_QUADEN|MX25L512_SR_WIP;// Same as
SST26VF032B
s_config.MatchMode = QSPI_MATCH_MODE_AND; s_config.StatusBytesSize = 1; s_config.Interval = 0x10; s_config.AutomaticStop = QSPI_AUTOMATIC_STOP_ENABLE;s_command.InstructionMode = QSPI_INSTRUCTION_4_LINES;
s_command.Instruction = READ_STATUS_REG_CMD; s_command.DataMode = QSPI_DATA_4_LINES;if (HAL_QSPI_AutoPolling(hqspi, &s_command, &s_config, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{ return QSPI_ERROR; }////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
I believe some configuration is wrong. Please help.
Thank you.
Regards,
Thiha Kyaw