cancel
Showing results for 
Search instead for 
Did you mean: 

PWM on TIM1

benoit
Associate
Posted on April 24, 2013 at 13:33

Hello everybody,

I ever look on webside if previous post treat my problem, but they not resolve my pb.

The problem is, I try to pramreter the TIM1 PWM output on STM32, but it do not work.

The TIM1 counter register CNT is counting realod, but it dosen't switch PA8. However the GPIOA IDR8 folow the overflow of CCR1.

This is my code :

GPIO_DeInit(GPIOA);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA|RCC_APB2Periph_AFIO, ENABLE);

RCC_APB2PeriphResetCmd(RCC_APB2Periph_GPIOA|RCC_APB2Periph_AFIO, DISABLE);

[...]

// PWM output

i=8;

GPIO_StructInit(&GPIOA_InitStruct[i]);

GPIOA_InitStruct[i].GPIO_Pin   = GPIO_Pin_8;

GPIOA_InitStruct[i].GPIO_Speed = GPIO_Speed_50MHz;

GPIOA_InitStruct[i].GPIO_Mode  = GPIO_Mode_AF_PP;                         // Alternate Fonction

GPIO_Init(GPIOA,&GPIOA_InitStruct[i]);

[...]

RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);                    

      RCC_APB2PeriphResetCmd(RCC_APB2Periph_TIM1, DISABLE);                    

     

      

      /* configures the timer 1 clock and divisors */

      TIM_DeInit(TIM1);

      

      TIM_1.TIM_Prescaler         = 550 ;           //550 => 1sec               // 36000000/9= 4 Mhz => periodes de 0.25µs

      TIM_1.TIM_Period            = 65535 ; //400                             

      TIM_1.TIM_ClockDivision     = TIM_CKD_DIV1;                             

      TIM_1.TIM_CounterMode       = TIM_CounterMode_Up;                        

      TIM_TimeBaseInit(TIM1,&TIM_1);                                          

      TIM_ARRPreloadConfig(TIM1, ENABLE);                                     

    /* Configures the TIM1 Channel1 */

      OC_TIM_1.TIM_OCMode = TIM_OCMode_PWM1;                                  

      OC_TIM_1.TIM_OutputState = TIM_OutputState_Enable;                      

      OC_TIM_1.TIM_OutputNState = TIM_OutputNState_Disable;                    

      OC_TIM_1.TIM_Pulse = 32768;                                                  

      OC_TIM_1.TIM_OCPolarity = TIM_OCPolarity_Low;                           

      OC_TIM_1.TIM_OCNPolarity = TIM_OCNPolarity_High;                         

      OC_TIM_1.TIM_OCIdleState = TIM_OCIdleState_Reset;                      

      OC_TIM_1.TIM_OCNIdleState = TIM_OCIdleState_Reset;                     

    

      TIM_OC1Init(TIM1, &OC_TIM_1);

      

      TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable);                       

      /* Enables the TIM counter */

      TIM_CtrlPWMOutputs(TIM1, ENABLE);                                        

      TIM_Cmd(TIM1, ENABLE);                                                 

Thank you for your help.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on April 24, 2013 at 13:39

      OC_TIM_1.TIM_Pulse = 0;   // << Always OFF, pick something like 32768 for 50/50 duty                                            

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
benoit
Associate
Posted on April 24, 2013 at 13:44

''OC_TIM_1.TIM_Pulse = 0;'' don't worry I'm not

thoughtless

, I modify after with TIM_SetCompare1.