2013-04-19 7:09 AM
Hi,
I need to replace a 5V-uC by a 3.3V type and maybe it will be a STM32F0xxx. Now there is one question concerning 5V tolerance: If the 3.3V-uC drives an output that has a pullup resistor to 5V, is that any problem because of current flowing into the output pin?
Thank you very much Martin2013-04-19 9:12 AM
yes. You do not drive the pin high.
logic low: You make the pin an output and drive it lowlogic high: You make the pin an input, then the 5v pull up resistor drives it highto toggle, just change the pin from input, to output, to input, ....2013-04-19 10:29 AM
if you are replacing a push-pull output with an output pulled up by a resisitor you will see greatly increased risetimes. sometimes a problem, sometimes not.
Erik2013-04-20 12:15 AM
You can configure pin as output open-drain so only N output transistor is activated when output is low.
2013-04-22 12:55 AM
Hi,
thank you for your answers. I was asking this question also to the ST online support and got no answer for quite a while, so I decided to post it here. As things are going I received an answer right after that. Just to complete it I also post it here: You should configure the GPIO as open drain and disable the internal pull-up (the external one only shall be used).When the FT pin is then output-low, there is max allowed current 25mA through the pin. In output-high guarantees the FT pin circuitry zero injection current when the external voltage applied to the pin is above VDD (and below VDD+4V).
As a conclusion I understand that I should not use the high side FET of the output. Just to improve my knowledge I would like to know what would or could happen if I configured the output as pushpull. Any hints on this would be welcome Thanks Martin2013-04-24 1:26 AM