2018-07-14 10:53 AM
hello;
I want to define the pinAO as a push button on keil v5 without using cubemx, i need its define and configuration function, can some one help?
2018-07-14 11:37 AM
{
GPIO_InitTypeDef GPIO_InitStructure;/* Enable GPIOA clock */
__HAL_RCC_GPIOA_CLK_ENABLE();/* Configure PA0 pin as input pulled up (pressed button connects to ground) */
GPIO_InitStructure.Mode = GPIO_MODE_INPUT; GPIO_InitStructure.Pull = GPIO_PULLUP; GPIO_InitStructure.Pin = GPIO_PIN_0; HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);//...
if (HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_0) == 0)
puts('Button Depressed');}2018-07-14 02:03 PM
,
,
This is the code that i wrote can u point it it compiling successfully, but its not working can u point out the errors , ?
♯ include 'stm32f4xx_hal.h'
,
void GPIO_CONFIGER(void),,
void PUSHBUTTON(void),,
int main(void){,
HAL_Init(),,
GPIO_CONFIGER(),,
PUSHBUTTON(),,
while(1){,
GPIO_PinState MY_PUSHBUTTON,,
,
MY_PUSHBUTTON=HAL_GPIO_ReadPin(GPIOA,GPIO_PIN_0),if(MY_PUSHBUTTON){
,
HAL_GPIO_WritePin(GPIOD,GPIO_PIN_12,MY_PUSHBUTTON),,
HAL_Delay(1000),,
HAL_GPIO_WritePin(GPIOD,GPIO_PIN_13,MY_PUSHBUTTON),,
HAL_Delay(1000),,
HAL_GPIO_WritePin(GPIOD,GPIO_PIN_14,MY_PUSHBUTTON),,
HAL_Delay(1000),,
HAL_GPIO_WritePin(GPIOD,GPIO_PIN_15,MY_PUSHBUTTON),,
HAL_Delay(1000),,
,
},
},
,
}void GPIO_CONFIGER(void){
,
__HAL_RCC_GPIOD_CLK_ENABLE(),,
,
GPIO_InitTypeDef GPIOPIN,,
GPIOPIN.Mode= GPIO_MODE_OUTPUT_PP ,,
GPIOPIN.Pin= GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15 ,,
HAL_GPIO_Init(GPIOD, &,GPIOPIN),}
,
void PUSHBUTTON(void){,
__HAL_RCC_GPIOA_CLK_ENABLE(),,
GPIO_InitTypeDef MYPUSHBUTTON,,
MYPUSHBUTTON.Pin=GPIO_PIN_0,,
MYPUSHBUTTON.Mode=GPIO_MODE_INPUT,,
MYPUSHBUTTON.Pull=GPIO_PULLUP,,
HAL_GPIO_Init(GPIOA,&,MYPUSHBUTTON),,
if(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_0)==0){,
puts('Button Depressed'),,
},
}void SYSTICK_CONGIR(){
,
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000),,
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK),,
HAL_NVIC_SetPriority(SysTick_IRQn,0,0 ),,
HAL_NVIC_EnableIRQ(SysTick_IRQn),}
void systick_handler(){
,
HAL_IncTick(),}