2017-02-24 05:10 AM
We need layout files of X-NUCLEO-IDW01M1
Solved! Go to Solution.
2017-02-25 06:19 AM
The Gerber format is an open ASCII vector format for 2D binary images. It is the de facto standard used by printed circuit board (PCB) industry software to describe the printed circuit board images: copper layers, solder mask, legend, etc.
2017-02-24 05:31 AM
Please refer to
on ST web site.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-02-24 05:32 AM
http://www.st.com/en/ecosystems/x-nucleo-idw01m1.html
Gerber files, schematic, and BOM are there if you scroll down
2017-02-24 10:49 PM
Can we get the layout file
On Fri, Feb 24, 2017 at 7:03 PM, john doe <st-microelectronics@jiveon.com>
2017-02-25 06:19 AM
The Gerber format is an open ASCII vector format for 2D binary images. It is the de facto standard used by printed circuit board (PCB) industry software to describe the printed circuit board images: copper layers, solder mask, legend, etc.
2017-02-27 04:07 AM
Ok,
We are using
STM32L152RET6
How to set up RTC.Is there any internal RTC?
On Sat, Feb 25, 2017 at 6:50 PM, john doe <st-microelectronics@jiveon.com>
2017-02-28 06:14 AM
Hello,
If the subject change, I suggest you to open a new discussion thread.
This will ease any research.
Kind regards
Sirma