cancel
Showing results for 
Search instead for 
Did you mean: 

programming the STM32L151CCT6

wl
Associate
Posted on December 08, 2015 at 10:34

I am trying to program the STM32L151 device using V2.8 of the Demonstrator GUI application.

I see that the device is already in BOOT mode because when i sniff the UART communications, the traces shows that the application is in communications. However, the GUI was not able to get the PID and the BID shows 0. And the Target list anything selectable.

The trace of the UART communications is shown at the bottom. What could be the problem. Thanks !!

Request: 12/8/2015 5:25:26 PM.68564 (+3281 seconds) 7F  Answer: 12/8/2015 5:25:26 PM.68564 (+0.0000 seconds) 79 y Request: 12/8/2015 5:25:26 PM.68564 (+0.0000 seconds) 00 FF .ÿ Answer: 12/8/2015 5:25:26 PM.68564 (+0.0000 seconds) 79 0B 31 00 01 02 11 21 31 44 63 73 82 92 79 y.1....!1Dcs‚’y Request: 12/8/2015 5:25:26 PM.68564 (+0.0000 seconds) 02 FD .ý Answer: 12/8/2015 5:25:26 PM.68564 (+0.0000 seconds) 79 01 04 27 79 y..'y Request: 12/8/2015 5:25:26 PM.68564 (+0.0000 seconds) 02 FD .ý Answer: 12/8/2015 5:25:26 PM.68564 (+0.0000 seconds) 79 01 04 27 79 y..'y Request: 12/8/2015 5:25:26 PM.70164 (+0.0156 seconds) 11 EE .î Answer: 12/8/2015 5:25:26 PM.70164 (+0.0000 seconds) 79 y Request: 12/8/2015 5:25:26 PM.70164 (+0.0000 seconds) 08 00 00 00 08 ..... Answer: 12/8/2015 5:25:26 PM.70164 (+0.0000 seconds) 79 y Request: 12/8/2015 5:25:26 PM.70164 (+0.0000 seconds) 03 FC .ü Answer: 12/8/2015 5:25:26 PM.70164 (+0.0000 seconds) 79 00 00 00 00 y.... Request: 12/8/2015 5:25:28 PM.12364 (+2.4219 seconds) 02 FD .ý Answer: 12/8/2015 5:25:28 PM.12364 (+0.0000 seconds) 79 01 04 27 79 y..'y Request: 12/8/2015 5:25:28 PM.12364 (+0.0000 seconds) 02 FD .ý Answer: 12/8/2015 5:25:28 PM.12364 (+0.0000 seconds) 79 01 04 27 79 y..'y Request: 12/8/2015 5:25:28 PM.12364 (+0.0000 seconds) 00 FF .ÿ Answer: 12/8/2015 5:25:28 PM.12364 (+0.0000 seconds) 79 0B 31 00 01 02 11 21 31 44 63 73 82 92 79 y.1....!1Dcs‚’y Request: 12/8/2015 5:25:28 PM.15464 (+0.0313 seconds) 11 EE .î Answer: 12/8/2015 5:25:28 PM.15464 (+0.0000 seconds) 79 y Request: 12/8/2015 5:25:28 PM.15464 (+0.0000 seconds) 1F F0 1F FE 0E .ð.þ. Answer: 12/8/2015 5:25:28 PM.15464 (+0.0000 seconds) 79 y Request: 12/8/2015 5:25:28 PM.15464 (+0.0000 seconds) 01 FE .þ Answer: 12/8/2015 5:25:28 PM.15464 (+0.0000 seconds) 79 40 00 y@.

2 REPLIES 2
wl
Associate

Posted on December 12, 2015 at 04:05

I had just changed the micro to STM32L151C6T6A version. Seems like it is also not supported by the ST demonstrator GUI programmer. The program hangs after selecting the target of STM32L1_Cat2-32K. The board is perfectly working with an STM32F103 series.

It is a shame that ST did not even ensure that the tools are workable when they claim it is a low power drop in replacement. So far, i had received zero reply or assistance.

This is the communications trace between the flashing and the microcontroller for those who may be interested (STM32L151C6T6).

7F  Answer: 12/12/2015 10:52:19 AM.70064 (+0.0000 seconds) 79 y Request: 12/12/2015 10:52:19 AM.70064 (+0.0000 seconds) 00 FF .ÿ Answer: 12/12/2015 10:52:19 AM.70064 (+0.0000 seconds) 79 0B 31 00 01 02 11 21 31 44 63 73 82 92 79 y.1....!1Dcs‚’y Request: 12/12/2015 10:52:19 AM.70064 (+0.0000 seconds) 02 FD .ý Answer: 12/12/2015 10:52:19 AM.71664 (+0.0156 seconds) 79 01 04 29 79 y..)y Request: 12/12/2015 10:52:19 AM.71664 (+0.0000 seconds) 02 FD .ý Answer: 12/12/2015 10:52:19 AM.71664 (+0.0000 seconds) 79 01 04 29 79 y..)y Request: 12/12/2015 10:52:19 AM.73264 (+0.0156 seconds) 11 EE .î Answer: 12/12/2015 10:52:19 AM.73264 (+0.0000 seconds) 79 y Request: 12/12/2015 10:52:19 AM.73264 (+0.0000 seconds) 08 00 00 00 08 ..... Answer: 12/12/2015 10:52:19 AM.73264 (+0.0000 seconds) 79 y Request: 12/12/2015 10:52:19 AM.73264 (+0.0000 seconds) 03 FC .ü Answer: 12/12/2015 10:52:19 AM.73264 (+0.0000 seconds) 79 00 00 00 00 y.... Request: 12/12/2015 10:52:21 AM.76364 (+2.0313 seconds) 02 FD .ý Answer: 12/12/2015 10:52:21 AM.76364 (+0.0000 seconds) 79 01 04 29 79 y..)y Request: 12/12/2015 10:52:21 AM.76364 (+0.0000 seconds) 02 FD .ý Answer: 12/12/2015 10:52:21 AM.76364 (+0.0000 seconds) 79 01 04 29 79 y..)y Request: 12/12/2015 10:52:21 AM.76364 (+0.0000 seconds) 00 FF .ÿ Answer: 12/12/2015 10:52:21 AM.76364 (+0.0000 seconds) 79 0B 31 00 01 02 11 21 31 44 63 73 82 92 79 y.1....!1Dcs‚’y Request: 12/12/2015 10:52:26 AM.45064 (+5.6719 seconds) 11 EE .î Answer: 12/12/2015 10:52:26 AM.45064 (+0.0000 seconds) 79 y Request: 12/12/2015 10:52:26 AM.45064 (+0.0000 seconds) 1F F0 0F FE 1E .ð.þ. Answer: 12/12/2015 10:52:26 AM.45064 (+0.0000 seconds) 79 y Request: 12/12/2015 10:52:26 AM.45064 (+0.0000 seconds) 01 FE .þ Answer: 12/12/2015 10:52:26 AM.45064 (+0.0000 seconds) 79 20 00 y .

_________________________

 Attachments :

DEMOGUIERR2.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I13c&d=%2Fa%2F0X0000000bhY%2Fq2uWlbDHwDEIbjdxqwJIZq.kd9ZnhkOF1lcGNrInaLs&asPdf=false

Posted on December 12, 2015 at 04:46

So far, i had received zero reply or assistance.

I should point out this is a user forum, if you want an FAE you'll need to use other channels.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..