2023-09-20 2:08 AM
Dear admin,
I would like to know which process technology (?nm) of STM32L4R9I-EVAL evaluation board.
I've checked the user manual but not having this information.
Thanks & Best Regards
Solved! Go to Solution.
2023-09-20 3:00 AM
Uhm, do you mean the minimum width of the tracks used to make the EVAL's board? Or maybe the structure width of the STM32L4R9AII6 used on the STM32L4R9I-EVAL?
If the latter, then this is a 90nm technology.
Regards
/Peter
2023-09-20 3:00 AM
Uhm, do you mean the minimum width of the tracks used to make the EVAL's board? Or maybe the structure width of the STM32L4R9AII6 used on the STM32L4R9I-EVAL?
If the latter, then this is a 90nm technology.
Regards
/Peter
2023-10-30 8:50 AM
Where can I find this information?
Unless I went too quickly I didn't see it in the RM or the datasheet.
The better source I find is Wikipedia! https://en.wikipedia.org/wiki/STM32
2023-10-30 9:12 AM
https://mm.digikey.com/Volume0/opasdata/d220001/medias/docus/4316/MDG-21-12467.pdf
https://www.anglia.com/registration/pcn_ptn/docs/pcn/st_PCN%20MDG_19_10816_Report.pdf