2010-09-15 12:14 AM
Problems with the ADC TIME CONVERSION
2011-05-17 5:07 AM
STM32f10xx_it.c
void TIM1_UP_IRQHandler(void) { GPIOA->BSRR = GPIO_Pin_4; /* Toggle PIN */ TIM1_ClearITPendingBit(TIM1_FLAG_Update); /* Clear UPDATE interrupt bit */ } void ADC_IRQHandler(void) { GPIOA->BRR = GPIO_Pin_4; /* Toggle PIN */ ADC1->SR = ~((u16)0x0004); /* Clear ADC interrupt bit */ } I code the main features like that.main.c
--------------------------------------------------------------------------------- --------------------------------------------------------------------------------- NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4); /* Sin Group Priority, PRI-n[7:4] Subpriority */ NVIC_SETPRIMASK(); /* DESHABILITA las interrupciones para configuracion */ /* Configure and enable ADC interrupt */ NVIC_InitStructure.NVIC_IRQChannel = ADC1_2_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = TIM1_UP_IRQChannel; /* TIM1 Update Interrupt */ NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; /* Valor de prioridad [0~15] */ NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; /* Valor de subprioridad */ NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; /* Habilita la interupción elegida */ NVIC_Init(&NVIC_InitStructure); NVIC_RESETPRIMASK(); /* HABILITA las interrupciones despues de configuracion */ --------------------------------------------------------------------------------- --------------------------------------------------------------------------------- RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_7); /* SYSCLK=56MHZ*/ RCC_ADCCLKConfig(RCC_PCLK2_Div4); /* ADC PCLK2/4=14MHz - CONFIGURE RCC_CFGR.ADCPRE */ RCC_PCLK2Config(RCC_HCLK_Div1); /* APB2 PCLK2 = 56MHz */ RCC_HCLKConfig(RCC_SYSCLK_Div1); /* AHB HCLK = 56MHz CONFIGURE RCC_CFGR.HPRE */ --------------------------------------------------------------------------------- --------------------------------------------------------------------------------- ADC_InjectedChannelConfig(ADC1, ADC_Channel_15, 1, ADC_SampleTime_1Cycles5);2011-05-17 5:07 AM
Hi Gerardo,
Why you don't use systick timer. I think it is useful for time measurement and perhaps it is more accurate than using GPIO. Herzlich, MCU Lüfter2011-05-17 5:07 AM
Anyone knows the answer?
Can it be the time lost going to the ISR? I´ve somo doubts with the TIM1 overflow interrupt, because i have to enable it only to see the exact time that ADC starts, not to work the ADC, only to know this time. May i doing it bad?2011-05-17 5:07 AM
I´ve tried it to see it in oscilloscope. I will investigate your way to do it and I will tell you if I get a solution.
Thks for replying!!2011-05-17 5:07 AM
Hi lowpower:
I tried what you say but i couldn´t achive any thing. I configure the systick with 3us time, to ensure that it nevers downflows.MI strategie is turn ON the systick system when the TIM1 overflows (like i did with toggle pin, but with systick timer). when the ADC finishes, I enter in its ISR, and then I turn OFF the systick timer. Then with a breakpoint and a debugger, I saw the register STK_VAL(Value of systick). I thought that this time of systick must be 1us but, when I enable the systick, my code never leaves the TIM ISR. If I delete the code it alternates TIM and ADC ISR. I´m getting a little bit confused. My configuration is the following:void TIM1_UP_IRQHandler(void) { SysTick_CounterCmd(SysTick_Counter_Enable); TIM1->SR &= ~ 1; /* Clears TIM1 FLAG */ }void ADC_IRQHandler(void) { SysTick_CounterCmd(SysTick_Counter_Disable); SysTick_CounterCmd(SysTick_Counter_Clear); ADC1->SR = ~((u16)0x0004); /* Clears ADC FLAG */ } Main.cSysTick_SetReload(168); /* A frecuencia de 56MHz 3uS */