2009-04-15 02:43 AM
problems with current consumption in stop mode
2011-05-17 04:09 AM
Hello,
I`m trying to measure stm32f103 power (current) consumption. In stop mode (VDD=3.3V) without RTC it ''eats'' 26uA and that`s perfect, but then I turn on RTC current consumption rise up to 82uA. According to datasheet I suppose it should not be bigger than 30uA. Has anybody some thoughts on this point?2011-05-17 04:09 AM
did you solve this issue?
I have the same problem: - 14uA STOP MODE RTC OFF - 28uA STOP MODE RTC ON Any clue?