Problems in sleep mode using STM32CubeHALv1.7.0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-09-27 5:29 AM
Hi,
I
use the
STM32L152RE
device
and
I
found some problems when I
execute
the sleep mode
in STM32CubeHALv1.7.0
.
In fact, w
hen I use the __HAL_PWR_VOLTAGESCALING_CONFIG function with PWR_REGULATOR_VOLTAGE_SCALE3 for
a
low frequenc
y (lower than 4MHz)
, this instruction
stops the
execut
ion
, while this function is executed for the two other
ranges
(PWR_REGULATOR_VOLTAGE_SCALE1 and PWR_REGULATOR_VOLTAGE_SCALE2). I tried to change the value of this variable
(PWR_REGULATOR_VOLTAGE_SCALE3)
from
PWR_CR_VOS (
0x00001800
)
to 0x0000C000. With this setting, the function runs.
P
lease, is it possible to check if there is an error
in the
definition
of this value?
In the other hand
, the HAL_RCC_DeInit
function
does not execut
e
. Indeed,
the
execution
is stopped
in
the function of switching the SYSCLK to MSI
(CLEAR_BIT(RCC->CFGR, RCC_CFGR_SW);)
. When, I
change this function CLEAR_BIT
by
SET_BIT
function
and change the order of the 4
th
instruction (Reset CFGR register) before
the instruction switch SYSCLK to MSI, the code is executed and the sleep mode
outperforms
the normal mode
in terms of energy consumption
.
P
lease, can you verify if there
are
some problem
s
in the function
HAL_RCC_DeInit
?
T
hank you in advance.
Best regards,
Wassim Ben Chikha
Note: this post was migrated and contained many threaded conversations, some content may be missing.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 12:28 AM
Hello!
I tried to change the value of this variable
(PWR_REGULATOR_VOLTAGE_SCALE3)
from
PWR_CR_VOS (
0x00001800
)
to 0x0000C000. With this setting,
This setting leaves VOS unchanged , sets the reserved bit 15 and also sets LPRUN bit14
For the second part of your question:
Please, can you verify if there are some problems in the function HAL_RCC_DeInit
It seems that HAL_RCC_DeInit function sets as systemclock the MSI , whithout check for MSIRDY flag in the RCC_CR register. Yes i thing this is a problem .
Regards
vf
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 2:56 AM
Hello Wassim,
Your reported issue about
HAL_RCC_DeInit
function
is raised internally for further review.All your comments and suggestions are welcome to improve our solutions.
Best Regards
Imen
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 5:00 AM
Hello Imen,
Many thanks for your time and consideration.
Kind regards,
Wassim Ben Chikha
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 8:01 AM
Hello Vangelis,
According to the RM0038 Reference manual, I agree with you that
changing the value of the variable
(PWR_REGULATOR_VOLTAGE_SCALE3)
from
PWR_CR_VOS (
0x00001800
)
to 0x0000C000, leaves VOS unchanged, sets the reserved bit 15 and also sets LPRUN bit14. But, the __HAL_PWR_VOLTAGESCALING_CONFIG function using PWR_REGULATOR_VOLTAGE_SCALE3 (0x00001800) stops the execution. Thus, I think that there is an error in the definition of this value.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 8:59 AM
Hello again!
But, the __HAL_PWR_VOLTAGESCALING_CONFIG function using PWR_REGULATOR_VOLTAGE_SCALE3 (0x00001800) stops the execution.
I checked the
__HAL_PWR_VOLTAGESCALING_CONFIG and according to RM sets or clears the VOS bits.
I will try later to find why stops the execution .I have a board with L152.
It would help a lot if you post some code here. Like an .IOC file and main func .
Regards
vf
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 9:21 AM
Hello again,
In fact, when I use the function SystemClock_Config implemented in cube_hal_l1.c file (V1.0.0, date: 03-November 2014) with
a
low frequenc
y (lower than 4MHz: 1, 2 or 4MHz), I found that __HAL_PWR_VOLTAGESCALING_CONFIG function using PWR_REGULATOR_VOLTAGE_SCALE3 (0x00001800) stops the execution. Please can you verify if there is a possibility that VOS[1:0]= 00 for range 3 and VOS[1:0]=11: forbidden (bits are unchanged and keep the previous value, no voltage scaling range changed)? Indeed, _HAL_PWR_VOLTAGESCALING_CONFIG function using PWR_REGULATOR_VOLTAGE_SCALE3 (0x00000000) is executed without any problem.
Many thanks for your time and look forward for you response.
Best regards,
WBC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 10:30 AM
Hello again.
Does your code wait for VOSF flag?
If not , due to system clock stopping, your debugger will disonnect.
Take some care to follow theese note about change voltage scalling.
Regards
vf
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 10:39 AM
Hi
wassimbenchikha
,I have tested and checked this case with
STM32L152REdevice
, but I'm not able to reproduce this behavior.Could you please share your code,so that it will be easier to understand the issue.
Kind Regards
Imen
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 10:55 AM