Problem with USART
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-15 12:31 AM
Posted on March 15, 2016 at 08:31
HI, I'm trying to develop a simple communication with my laptop sending just one character, the problem is that I need to send the character more than 5 times for reconogise it in the Discovery board, the code is simple.
void USART1init(){usart1.Instance = USART1;usart1.Init.BaudRate = 9600;usart1.Init.WordLength = USART_WORDLENGTH_8B;usart1.Init.StopBits = USART_STOPBITS_1;usart1.Init.Parity = USART_PARITY_NONE;usart1.Init.Mode = USART_MODE_TX_RX;usart1.Init.CLKPolarity = USART_POLARITY_LOW;usart1.Init.CLKPhase = USART_PHASE_1EDGE;usart1.Init.CLKLastBit = USART_LASTBIT_DISABLE;HAL_USART_Init(&usart1);}void USART1_Pins_Init(){ RCC->AHB1ENR|=RCC_AHB1ENR_GPIOAEN;//Damos reloj al GPIO RCC->APB2ENR|=RCC_APB2ENR_USART1EN;//Damos reloj al USART1 //__USART1_CLK_ENABLE(); GPIO_InitTypeDef GPIO_InitStruct; GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Alternate = GPIO_AF7_USART1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);}void Read_Usart1(){ uint8_t Buffer=0; uint16_t Size=1; uint32_t Timeout=500; HAL_USART_Receive(&usart1,&Buffer,Size,Timeout); if (Buffer=='B')Led_ON(); if (Buffer=='C')Led_OFF();}
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-15 2:34 AM
Posted on March 15, 2016 at 10:34
Ok, and which of the dozens of different discovery boards would this be?
The STM32F407-DISCO would have a problem with PA9 due to VERY large capacitor. Does it work better at 1200 baud?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-15 3:15 AM
Posted on March 15, 2016 at 11:15
Thanks, my board is the STM32 discovery 429-DISC0
I´ve checked it at 1200 baud and it doesn´t work,this time don´t recive anything