cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with UART RTS

NToua.2461
Associate II

HI ?

i work with STM32F103CB ,The problem is the STM does not toggle the RTS. RTS still tied high i can't find the problem can someone help me please.

we found here my code.

void USART_GPIO_Init(void)

{

  // Configuration of GPIOA clock source

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE);

RCC-> APB2RSTR =0;

GPIO_PinRemapConfig(GPIO_Remap_USART1 , DISABLE) ;

  /* Enable the USART periph */

RCC_APB2PeriphClockCmd( RCC_APB2Periph_USART1, ENABLE);

GPIO_InitTypeDef GPIO_InitStructure;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;//GPIO_Mode_AF_PP;

GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 |  GPIO_Pin_12 ;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;//GPIO_Mode_IN_FLOATING;

GPIO_Init(GPIOA, &GPIO_InitStructure);

}

void FTDI_Init(void)

{

USART_InitTypeDef  USART_InitStructure;

RCC_APB2PeriphClockCmd( RCC_APB2Periph_USART1, ENABLE);

USART_InitStructure.USART_BaudRate = 9600;

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No ;

USART_InitStructure.USART_Mode = USART_Mode_Tx|USART_Mode_Rx;

USART_InitStructure.USART_HardwareFlowControl =USART_HardwareFlowControl_RTS_CTS;

USART_Init( USART1, &USART_InitStructure);

    NVIC_InitTypeDef NVIC_InitStructure;

  NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 5;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

USART_ITConfig(USART1, USART_IT_RXNE,ENABLE);

  __enable_irq();

 USART_Cmd(USART1, ENABLE);

}

Interruption code :

void USART1_IRQHandler(void)

 {

if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET)

{

for(Ri=0 ; Ri<5 ; Ri++)

{

DATA_receive = USART_ReceiveData(USART1);

buffer[Ri] = DATA_receive;

}

}

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0