cancel
Showing results for 
Search instead for 
Did you mean: 

Problem running STM32CubeProgrammer

adavide
Associate

When running the program STM32CubeProgrammer, an error message appears, saying:

"CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program of check your java architecture". However I have the lastest JAVA SE Run Time installed.

Any idea?

OS:

Windows 10 64-bit

Java: 1.8.0_192-b12

STM32CubeProgrammer version: 1.4.0

1 REPLY 1
Uwe Bonnes
Principal III

Welcome to the Java version hell! I only got the programmer working on one of two Linux machines, and that machine does not recognize the STLINK V3.

The error message is also not helpfull. If it would tell _what_ is not found, own research could be done.