cancel
Showing results for 
Search instead for 
Did you mean: 

Problem programming with STM32CubeProgrammer

AKoci
Associate

Hi,

I'm trying to programm a Viasala RS41 radiosonde with STM32 Cube Programmer. I'm following instructions from some other people who did this already. But when I try to programme the chip, I get only an error:

Error: Failed to erase memory

This ist the Log:

21:22:31 :

21:22:31 : Memory Programming ...

21:22:31 : Opening and parsing file: C:\Temp\rtty.hex

21:22:31 :  File         : C:\Temp\rtty.hex

21:22:31 :  Size         : 62704 Bytes

21:22:31 :  Address      : 0x08000000

21:22:31 :

21:22:31 : Erasing Segment <0> Address <0x08000000> Size <62704>Bytes

21:22:31 : Erasing memory corresponding to segment 0:

21:22:31 : Memory erase...

21:22:31 : reset ap 0

21:22:31 : run ap 0

21:22:31 : halt ap 0

21:22:31 : w ap 0 reg 15 (0x20000000) 

21:22:31 : w ap 0 reg 17 (0x20000500) 

21:22:31 : w ap 0 reg 16 (0x01000000) 

21:22:31 : w ap 0 @0x20000960 0x00000200 bytes

21:22:31 : w ap 0 @0x20000000 0x00000004 bytes

21:22:31 : w ap 0 @0x20000004 0x0000053E bytes

21:22:31 : Erasing internal memory sectors [0 61]

21:22:31 : Init flashloader...

21:22:31 : halt ap 0

21:22:31 : w ap 0 reg 0 0x00000001

21:22:31 : w ap 0 reg 1 0x00000000

21:22:31 : w ap 0 reg 2 0x00000000

21:22:31 : w ap 0 reg 3 0x00000000

21:22:31 : w ap 0 reg 4 0x00000000

21:22:31 : w ap 0 reg 5 0x00000000

21:22:31 : w ap 0 reg 6 0x00000000

21:22:31 : w ap 0 reg 7 0x00000000

21:22:31 : w ap 0 reg 8 0x00000000

21:22:31 : w ap 0 reg 9 0x00000000

21:22:31 : w ap 0 reg 10 0x00000000

21:22:31 : w ap 0 reg 11 0x00000000

21:22:31 : w ap 0 reg 12 0x00000000

21:22:31 : w ap 0 reg 13 0x00000000

21:22:31 : w ap 0 reg 14 0x20000001

21:22:31 : w ap 0 reg 15 0x20000005

21:22:31 : w ap 0 reg 16 0x01000000

21:22:31 : w ap 0 reg 17 0x2000093E

21:22:31 : w ap 0 reg 18 0x00000000

21:22:31 : run ap 0

21:22:31 : halt ap 0

21:22:31 : r ap 0 reg 0 0x00000001

21:22:31 : Loader sector erase...

21:22:31 : w ap 0 reg 0 0x08000000

21:22:31 : w ap 0 reg 1 0x0800F400

21:22:31 : w ap 0 reg 2 0x00000002

21:22:31 : w ap 0 reg 3 0x00000000

21:22:31 : w ap 0 reg 4 0x00000000

21:22:31 : w ap 0 reg 5 0x00000000

21:22:31 : w ap 0 reg 6 0x00000000

21:22:31 : w ap 0 reg 7 0x00000000

21:22:31 : w ap 0 reg 8 0x00000000

21:22:31 : w ap 0 reg 9 0x00000000

21:22:31 : w ap 0 reg 10 0x00000000

21:22:31 : w ap 0 reg 11 0x00000000

21:22:31 : w ap 0 reg 12 0x00000000

21:22:31 : w ap 0 reg 13 0x00000000

21:22:31 : w ap 0 reg 14 0x20000001

21:22:31 : w ap 0 reg 15 0x200001AF

21:22:31 : w ap 0 reg 16 0x01000000

21:22:31 : w ap 0 reg 17 0x2000093E

21:22:31 : w ap 0 reg 18 0x00000000

21:22:31 : run ap 0

21:22:31 : halt ap 0

21:22:31 : r ap 0 reg 0 0x00000000

21:22:31 : Error: failed to erase memory

21:22:31 :

21:22:31 : Error: failed to erase memory

The Sonde is connected through a ST-LINK V2 Interface.

The Cube Programmer seems to be conencted to the chip also.

Device Information says:

Device: STM32F100 Low/Medium densit...

Type: MCU

Device ID: 0x420

CPU: Cortex-M3

I have alreade disabled the read out protection in the settings.

But I can't imagine, why there is a problem erasing the memory.

How can I find out more about this problem, and has anyone an idea how to fix this?

If you need more information, just ask.

I'm not a professional programmer an I didn't do such a programming before.

Thanks in advance for any help.

Attila

2 REPLIES 2

Try updating the ST-LINK firmware to current

Try using ST-LINK Utilities instead

https://www.st.com/en/development-tools/stsw-link004.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AKoci
Associate

Thanks for this hint. It worked with this tool.

The Firmware has been updated already.

Thanks again! You made my day :)