Skip to main content
Iman Hosseinzadeh
Associate III
July 21, 2017
Question

Problem in setting CHSELR register

  • July 21, 2017
  • 0 replies
  • 1052 views
Posted on July 21, 2017 at 12:01

Following the previous post: 

https://community.st.com/0D50X00009XkYamSAF

 I tried to debug my program. 

The program has two steps.

1- Setting PA1, PA2 and PA3 as GPIO and reading ADC_CHANNEL_0

Waiting...

2-

Setting 

PA0, PA1 and PA3 as GPIO

and reading ADC_CHANNEL_2.

Waiting...

To select the ADC channel 0, we should set the following register to 0x1:

 ADC1->CHSELR = ADC_CHSELR_CHSEL0; // or = 0x1;

To select the ADC channel 2, we should set the following register to 0x4:

 ADC1->CHSELR = ADC_CHSELR_CHSEL4; // or = 0x4;

When I watch this register in debug mode, its value is set correctly in the first step. But in the second step its value is set to 5. (Actually the first bit does not reset.).

I also used the HAL libraries. HAL_ADC_ConfigChannel(&hadc, &sConfig) routine works fine individually. (I mean running only one step at once.) But running two steps consequently, rises the same problem.

I don't know what is the problem. 

#channel #adc #chselr
This topic has been closed for replies.