2017-12-11 02:29 PM
I am currently porting my project -
? - to STM32L4 family, so I wanted to download all the reference manuals. However I cannot download RM0351 - a RM for STM32L4x5 and STM32L4x6. If I start the download of the pdf file directly, it stops after exactly 4 MB and after some time the connection is broken. If I select the checkbox next to this document and click on the 'Download' button, the downloaded zip file contains the Japanese version (no matter which checkbox I choose, it's even the same when I choose both). If I google the name of the document and try to download it this way, it's exactly the same, even though the address is slightly different. Is this a local problem of my PC/network/ISP/whatever, or maybe someone else is having the same issue?Link to the reference manuals of STM32L4 family -
Link to the problematic file -
http://www.st.com/resource/en/reference_manual/dm00083560.pdf
#stm32l4 #documentation #reference-manual2017-12-11 06:23 PM
https://drive.google.com/open?id=12RjcXeTwlD91lTLkZrXtabytfpYnZNkJ
The server has been somewhat problematic in recent times. It seemed to download this evening ok, might be some caching issue. Attached is my mirror
2017-12-12 12:29 AM
OK, thanks for the file (; Let's hope the server issues will be resolved soon!