2021-10-03 10:26 AM
I am new to STM32. I am porting my code from ATMega128 to STM32 for faster thru put . I have to connect W5500 to STM32F103 on SPI2.
To test my understanding of SPI on STM32 after compiling , a small test code in while loop.
SPI_Write(S0_CR,CR_CLOSE); //#define S0_CR 0x0001, CR_CLOSE 0x10;
data_read = SPI_Read(S0_CR);
used the below sub functions
void SPI_Write(int addr,char data)
{
SPI_select
HAL_SPI_Transmit(&hspi2, ((addr & 0xFF00) >> 8), 1, 100);
HAL_SPI_Transmit(&hspi2, (addr & 0x00FF),1,100);
HAL_SPI_Transmit(&hspi2, (WRITE_OPCODE_S0),1,100);
HAL_SPI_Transmit(&hspi2, data, 1, 100);
SPI_deselect
}
char SPI_Read(int addr)
{
SPI_select
HAL_SPI_Transmit(&hspi2,((addr & 0xFF00) >> 8),1,100);
HAL_SPI_Transmit(&hspi2,(addr & 0x00FF),1,100);
HAL_SPI_Transmit(&hspi2,(READ_OPCODE_S0),1,100);
HAL_SPI_Receive(&hspi2,spi_rec,1,100);
SPI_deselect
return spi_rec;
}
Expected 0x10 (16) in data_read but got zero. thru UART. Tried diagnosing with
if(Err !=HAL_OK)
SPI_Write works to HAL_OK when first line address is not 0x00;
DSO Shows no SCK pulses when it is 0x00 though CS goes low.
Similarly in SPI_Read; line -- HAL_SPI_Receive(&hspi2,spi_rec,1,100); gives !=HAL_OK on UART
My proceeding further depends on clearing these doubts. Request help please.
Solved! Go to Solution.
2021-10-06 12:17 AM
The problem is solved.
The error was because I did not add a Ampersand & prefixed to uint8_t spi_rec in HAL_SPI_Receive(&hspi2, &spi_rec,1,100)
Now the HAL_OK comes thru till the last stage successfully thru UART.
Thanks a ton
2021-10-03 11:20 AM
> HAL_SPI_Transmit(&hspi2, ((addr & 0xFF00) >> 8), 1, 100);
> HAL_SPI_Transmit(&hspi2, (addr & 0x00FF),1,100);
> HAL_SPI_Transmit(&hspi2, (WRITE_OPCODE_S0),1,100);
> HAL_SPI_Transmit(&hspi2, data, 1, 100);
It looks like you're trying to send raw data in the first 3 function calls and a pointer to data in the last call. That's not how this function works. You need to provide a pointer to data. One way to do that is the following:
uint8_t value = (addr & 0xFF00) >> 8;
HAL_SPI_Transmit(&hspi2, &value, 1, 100);
value = addr & 0x00FF;
HAL_SPI_Transmit(&hspi2, &value, 1, 100);
value = WRITE_OPCODE_S0;
HAL_SPI_Transmit(&hspi2, &value, 1, 100);
It's unclear how data and spi_rec are defined.
2021-10-04 9:02 AM
Thanks for the response.
data_read and spi_rec have been declared as char.
Tried the method recommended on SPI_Read(S0_SR) but always gives Zero. S0_SR being the Socket Status Register where Zero could mean Socket closed or no value.
Still unable to resolve.
2021-10-04 9:45 AM
The code you posted should give you compiler errors. The second argument needs to be a pointer, not a char.
error: invalid conversion from 'char' to 'uint8_t* {aka unsigned char*}' [-fpermissive]
HAL_UART_Transmit(nullptr, data, 1, 100);
^
2021-10-04 8:03 PM
No Such compiler error threw up. However on your advice declared : uint8_t *spi_rec ;
To track the fault, changed the two sub-functions with if(err != HAL_OK) and used UART1 to check for any error.
if(err != HAL_OK) on the first line of both functions were avoided since the addr only contains 0x00 were no SCK pulses appear on DSO
void SPI_Write(int addr,char data)
{
char err;
SPI_select //HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET);
uint8_t value = (addr & 0xFF00) >> 8;
err = HAL_SPI_Transmit(&hspi2, &value, 1, 100);
value = addr & 0x00FF;
err = HAL_SPI_Transmit(&hspi2, &value, 1, 100);
if(err != HAL_OK)
{
strcpy(tx_buf,"Tx2 ? \r\n");
}
else
{
value = (READ_OPCODE_S0);
err = HAL_SPI_Transmit(&hspi2, &value, 1, 100);
if(err != HAL_OK)
{
strcpy(tx_buf,"Tx3 ? \r\n");
}
else
{
value = data;
err = HAL_SPI_Transmit(&hspi2,&value, 1, 100);
if(err != HAL_OK)
{
strcpy(tx_buf,"Tx4 ? \r\n");
}
else
sprintf(tx_buf,"Tx All OK data %d \r\n",data);
}
}
SPI_deselect
HAL_UART_Transmit(&huart1,tx_buf,strlen(tx_buf), 100);
}
uint8_t SPI_Read(int addr)
{
uint8_t err;
SPI_select //HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET);
uint8_t value = (addr & 0xFF00) >> 8;
err = HAL_SPI_Transmit(&hspi2, &value, 1, 100);
value = addr & 0x00FF;
err = HAL_SPI_Transmit(&hspi2, &value, 1, 100);
if(err != HAL_OK)
{
strcpy(tx_buf,"Rx2 ? \r\n");
}
else
{
value = (READ_OPCODE_S0);
err = HAL_SPI_Transmit(&hspi2, &value, 1, 100);
if(err != HAL_OK)
{
strcpy(tx_buf,"Rx3 ? \r\n");
}
else
{
err = HAL_SPI_Receive(&hspi2,spi_rec, 1, 100);
if(err != HAL_OK)
{
strcpy(tx_buf,"Rx4 ? \r\n");
}
else
sprintf(tx_buf,"Rx All OK %d \r\n",spi_rec);
}
}
SPI_deselect
HAL_UART_Transmit(&huart1,tx_buf,strlen(tx_buf), 100);
return spi_rec;
}
The while loop now had:
SPI_Write(S0_CR,CR_LISTEN); // CR_LISTEN
sockstat = SPI_Read(S0_SR); //#define S0_SR
where
#define S0_CR 0x0001 // Socket 0: Command Register Address in W5500
#define S0_SR 0x0003 // Socket 0: Status Register Address
#define CR_LISTEN 0x02 // Wait connection request in tcp mode(Server mode)
The Br@y Terminal showed:
Tx All OK data 2
Rx4 ?
Tx All OK data 2
Rx4 ?
Tx All OK data 2
Rx4 ?
I changed SPI2 configuration in GPIO settings of PB14 (MISO), though in input mode to Pull up --if anything changed in HAL_SPI_Receive ------Nothing changed.
Rx4 ? ------------------------still.
Just going in circles.
2021-10-04 8:13 PM
Maybe start with figuring out why your compiler is silently converting (char) to (uint8_t *) without errors. Then correct the usages of HAL_SPI_Receive where you're still passing a char.
> I changed SPI2 configuration in GPIO settings of PB14 (MISO), though in input mode to Pull up
Relevant SPI pins should be in AF mode.
If HAL_SPI_Receive isn't returning HAL_OK, what is it returning instead? It should not be a mystery. Figure out the return code and use that to help debug.
2021-10-05 12:22 AM
With Regards to your 2nd line, SPI2 set up --- PB14(MISO) always showed up as GPIO mode to Input while MOSI and SCK showed up as AF. Only I had changed to Pull up.
Now reverted back to No pull up or down . Should the MISO also show up as AF ?. ( which I am unable to change to AF)
As per your instructions, error in HAL_SPI_Receive is returning 1 which is HAL_ERROR. My understanding is { HAL_OK = 0x00U, HAL_ERROR = 0x01U, HAL_BUSY = 0x02U, HAL_TIMEOUT = 0x03U }; --- on google search.
Regards to your first Line-- Compiler silently converting (char) to (uint8_t *) without errors. Since I don't know how to go about it, I just converted Char to uint8_t
Problem not yet solved. Thanks for the quick response.
2021-10-06 12:17 AM
The problem is solved.
The error was because I did not add a Ampersand & prefixed to uint8_t spi_rec in HAL_SPI_Receive(&hspi2, &spi_rec,1,100)
Now the HAL_OK comes thru till the last stage successfully thru UART.
Thanks a ton