2017-04-16 08:39 AM
Thank you for your patronage. Please tell me how to calculate the dead time or determine dead time in this figure.
I understand that
HCLK = 84MHz
Prescaler = 83
Counter Period = 99
Pulse = 20
Dead Time = 150
so frequency = 10kHz, Duty ratio = 20%.
But I can't understand dead time is 2?s.
#dead-timeSolved! Go to Solution.
2017-04-18 03:20 PM
Basically it should be like 1/84000000 = 11.9ns. So you can have deadtime between 0 and 1511ns (11.9*127) with 11.9ns steps.
So for 2us, deadtime value should be like 168.
Thats what i think.
2017-04-16 05:16 PM
No dead time is defined
2017-04-17 03:58 AM
I'm sorry. Dead time =150.
2017-04-18 03:20 PM
Basically it should be like 1/84000000 = 11.9ns. So you can have deadtime between 0 and 1511ns (11.9*127) with 11.9ns steps.
So for 2us, deadtime value should be like 168.
Thats what i think.
2017-04-18 05:21 PM
this assumes Tdts = internal clock..
2017-04-20 04:24 AM
Thank you very much.