cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32F7] Use LSE as Timer source

Aaron Pica
Associate III
Posted on April 20, 2017 at 13:42

I'd like to use the LSE to clock an internal Timer. I had this implementation in some L1 devices, but I think this feature is missing with F7.

  • With L1 I had TIM10 with ETR2 as clock souce + ETR remaped to use LSE.
  • In F7, the ETR feature only allows getting the source from an external pin (TIMx_ETR) in TIM1/TIM2/TIM3/TIM4/TIM5/TIM8. The other timers (TIM6/TIM7/TIM9/TIM10/TIM11/TIM12/TIM13/TIM14) don't have this option.

Is the LPTIM1 the only way to use the LSE as a clock source? Am I missing something?

Thank you

#stm32f7 #timer #lse
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0