2013-02-13 07:04 AM
I am fairly new to this, so this might seem like a very basic question. Is there diagram of which GPIO pins can be connected to which alternate functions?
For instance something that shows which pins can be used as PWM/DAC/ADC/EXTI? or if there is no block diagram but maybe just some general conventions that I don't know maybe a quick walk through on the architecture.The specific device I'm using is the STM32F407VG. Any help would be appreciated.2013-02-13 07:15 AM
The pins are enumerated in the data manual, people have built Excel sheets.
ST has this MicroXplorer toolhttp://www.st.com/internet/evalboard/product/251717.jsp
2013-02-13 07:18 PM
Download the Datasheet and go to Table 6 on page 49:
http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/DM00037051.pdf