cancel
Showing results for 
Search instead for 
Did you mean: 

Pin Conifguration/Alternate function Map

berge472
Associate II
Posted on February 13, 2013 at 16:04

I am fairly new to this, so this might seem like a very basic question. Is there diagram of which GPIO pins can be connected to which alternate functions?

For instance something that shows which pins can be used as PWM/DAC/ADC/EXTI? or if there is no block diagram but maybe just some general conventions that I don't know maybe a quick walk through on the architecture.

The specific device I'm using is the STM32F407VG.  Any help would be appreciated.
2 REPLIES 2
Posted on February 13, 2013 at 16:15

The pins are enumerated in the data manual, people have built Excel sheets.

ST has this MicroXplorer tool

http://www.st.com/internet/evalboard/product/251717.jsp

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ken239955
Associate II
Posted on February 14, 2013 at 04:18

Download the Datasheet and go to Table 6 on page 49:

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/DM00037051.pdf