2025-07-31 9:58 PM - last edited on 2025-08-01 1:21 AM by Andrew Neil
Hi,
Could someone please explain the meaning of this image? It's a snapshot from CubeMX GPIO section.
Does it imply that PA12 and PA10 can be used as a single pin, or does it mean something else?
2025-07-31 10:32 PM
The reason I am asking is I am not able to Turn ON OR Toggle the pin PA12 I don't understand the reason why this pin gives me problem
2025-08-01 4:54 AM
By default, those pins are PA11 and PA12. You can set them as PA9 and PA10 instead with these checkboxes: