Performance of STM32F7 USB Mass Storage (MSC) <-> DMA <-> SD
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-25 2:50 AM
Posted on October 25, 2016 at 11:50
Hello everyone,
I am implementing a SD card-reader like device on my custom board with STM32F756 with SW4STM32 (AC6).Up to this date, I have successfully completed a working link to read/write file from the PC to SD card via my custom board with 4-bit SDIO & DMA. However, my problem here is the PERFORMANCE.The read/write speed are so low:Read from SD card: 1.35MB/s
Write to SD card: 158KB/s
I have ruled out SD card issue as it is a Class 4 SDHC which I can read @ 22MB/s and write @4.25MB/s using a common SD card reader off the shelf.Both my USB, SDIO clocks are set to the highest possible with the block size at 512.
Any idea where should I look into for performance improvement?
Anyone has tried using it on the official development board - STM32756G-EVAL or STM32746-EVAL? and how is the performance?
Do share your experience :) Thank you
3 REPLIES 3
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-25 10:51 AM
Posted on October 25, 2016 at 19:51
Hello,
Refer to this about STM32F7 performance, it may help you.RegardsOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-25 11:14 AM
Posted on October 25, 2016 at 20:14
Not sure that would go anywhere to explain the level of suck being reported here...
The read side suggests it is using USB-HS, the write numbers suggest it is writing single sectors.I'd instrument and understand the write patterns at the SDIO layer.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-26 1:14 AM
Posted on October 26, 2016 at 10:14
Some updates:
I have probed the SD Clock to make sure it is running at 48MHzSetup another test focusing on SD write by creating and write a big 10MB file into the SD card directly from the MCU without the activation of USB. The result I got was so bad, it just passed 100KB/s Is is possible to be caused by the skew? or the trace capacitance/ inductance/ impedance? To be honest, I wasn't giving too much attention to the layout design at this prototyping board stage.Regards,sy.t