2012-08-22 5:09 AM
The following code (TIM3 has clock enabled in RCC but otherwise is in its reset state):
#define TEST_TG
#ifdef TEST_TG TIM3->DIER |= TIM_DIER_TIE; // enable interrupt from trigger TRGI #else TIM3->DIER |= TIM_DIER_UIE; // enable interrupt from update event #endif testA[0] = NVIC_GetPendingIRQ(TIM3_IRQn); // there's no pending IRQ at the moment testA[1] = TIM3->SR; #ifdef TEST_TG TIM3->EGR = TIM_EGR_TG; // generate a trigger event #else TIM3->EGR = TIM_EGR_UG; // generate an update event #endif testA[2] = NVIC_GetPendingIRQ(TIM3_IRQn); // there should be a pending IRQ here in NVIC testA[3] = TIM3->SR; // and we should see it also on the status register __asm(''nop''); // okay, it may take time until the interrupt flags ''propagate'' to the __asm(''nop''); testA[4] = NVIC_GetPendingIRQ(TIM3_IRQn); // there should still be a pending IRQ in the NVIC testA[5] = TIM3->SR; // but not in the status register of the timer #ifdef TEST_TG TIM3->SR &= ~TIM_SR_TIF; // this clears the status bit #else TIM3->SR &= ~TIM_SR_UIF; // this clears the status bit #endif // the key to the problem is the number of cycles elapsed between these two events - >6 is needed to remove the problem in this snippet __asm(''nop \n\t nop \n\t nop \n\t nop \n\t nop \n\t nop \n\t''); // __asm(''nop''); NVIC_ClearPendingIRQ(TIM3_IRQn); // and this should clear the pending interrupt testA[6] = NVIC_GetPendingIRQ(TIM3_IRQn); // there should be no pending IRQ in the NVIC by now testA[7] = TIM3->SR; // __asm(''nop''); __asm(''nop''); __asm(''nop''); __asm(''nop''); testA[8] = NVIC_GetPendingIRQ(TIM3_IRQn); // and it should remain so testA[9] = TIM3->SR; // while(1) { __asm(''nop''); } results in(gdb) p /x testA
$26 = {0x0, 0x0, 0x0, 0x40, 0x1, 0x40, 0x0, 0x0, 0x1, 0x0} i.e. the ''pending'' bit ''reappears'' several cycles after having been cleared. If the ISR is enabled in NVIC after this sequence, this results in the respective ISR being fired without any bit indicating the source of interrupt set in the _SR. This is similar to the DMA pending problem I reported earlier in https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fHow%20to%20clear%20pending%20DMA%20request&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=35 Jan Waclawek