2014-07-17 07:46 AM
Would it be possible to connect to a PCIe device using an STM32F4? I'm looking to connect a cellular modem to an upcoming board, and most of the ones suitable for plugging into an embedded board (rather than soldering on an LGA package) come with a mini PCIe interface. The typical USB modems you get at Verizon aren't really suited for my application.
Thanks, Jeff. #stm32f4-pcie2014-07-17 08:42 AM
Don't they just export a USB interface? Then you'd still have to host it.
2014-07-17 11:11 AM
> Don't they just export a USB interface? Then you'd still have to host it.
Looks like some do, thankfully. I did find the Telit DE910 Mini PCIe that does.Thanks for the response.2014-07-17 11:51 AM
When that doesn't work out, let me know