2025-02-11 08:17 PM
I am using the controller STM32G491MCT controller for my development project.I am running out of GPIO pins.I am planning to use PC13 to drive the level translator SN74LV4T125 for sending serial clock and data signals from my master device to the slave module. It is given in the datasheet that there is some limitations in the PC13,PC14 & PC15 pins which cannot be used for driving high speed signals.
Could you please confirm that can I use the PC13 for driving level translator?
Anticipating the earliest response!
Thanks in advance