cancel
Showing results for 
Search instead for 
Did you mean: 

OTA update

YOrop.1
Associate

I would like to know if the following is possible and if so, where can I find information about it.

I have a STM32L010K8 micro connected via USART to an LTE CHIP (BG96) through which I can get the firmware update that runs on the microcontroller. I could overwrite the firmware of the micro STM32 to update it automatically.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Mostly limited by your own creativity and capabilities.

Should be able to pull data via modem using HTTP, FTP or other protocols.

You'd probably want to have a small, minimal, loader capable to connecting and updating, outside of the larger application.

Do you have any local memory with which to stage complete updates?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for the reply.

The BG96 has physical memory where I can store the firmware update for the microcontroller that I receive via HTTP.