One bit shift in SPI communication on STM32G4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-03 11:16 PM
Hi,
I am working on SPI communication between STM32G491 and ATM90E26. and I am using the SPI polling API with HAL_SPI_Transmit and HAL_SPI_Receive.
My System clock is 96Mhz and I am using prescaler of 64 for SPI.
CLKPolarity=Low,
CLKPhase=1Edge.
Communication is happening between the devices but I am not getting the correct data.
there is only a shift of one bit.
For example
in binary:
expected: 0001 0011 1001 0100
received: 0000 1001 1100 1010
f I shift the received bitstream to the left I get exactly the right result.
I found one solution in the forum for similar type of question(for stm32H7) It was solved with
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE;
But I am using STM32G4 with SPI Poll method
there is no MasterKeepIOState parameter available its giving me the error I use it.
Is it due to bad configutation?
or anything do I need to configure to solve it. Can anyone please suggest.
Thanks
Solved! Go to Solution.
- Labels:
-
STM32G4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-05 8:04 AM
Note that SPI is a bit exchange protocol. For every bit you send you receive a bit. So, given the "SPI sequence" you show you must transmit 3 bytes in order to properly set the register address and transfer the 2 data bytes (for either a read or write operation). You must use a 3-byte HAL_SPI_TransmitReceive() for the register read operation.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-03 11:49 PM
Hello @sireevenkat1
I suggest you to try to compare your exemple to one of those exemples.
Else, you can take a look at the UM2570 to find all SPI commands.
Best regards
II
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-04 5:46 AM
Normally this problem is due to a SPI clock signal integrity issue. Ensure the SPI clock is clean with minimal switching artifacts, reflections, etc.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-04 9:36 PM
Thanks for the replies @David Littell @Issamos ,
I changed SPI prescaler from 64 to 256 ,Now I can able to read correct values from few registers(ATM90E26 is energy meter IC).Now I can able to read frequency & meter status registers correctly. But If I read voltage and current registers I am always getting value zero values.
In ATM90E26 datasheet SPI Interface Bit Rate max is 160K Bps.
In my configuration 96Mhz(system clock)/256(prescaler)=375 kbps.
Is the issue with Bit rate? Can anyone clarify me ?
Because I can able to read few registers of ATM90E26 correctly & few registers I can't able to read.
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-04 11:49 PM
Hello again
I suggest you to reduce your bit rate and retry.
Best regards.
II
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-05 12:21 AM
Hi,
I did that still same issue.
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-05 12:38 AM
Then the issue is not caused by the baud rate. I suggest you to share your code here so the community members may help you finding your problem.
Best regards.
II
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-05 1:44 AM - edited ‎2023-09-05 1:46 AM
Hi,
Fully I can't share
I am sharing the logic
//write logic
void ATM90E26_SPI_Write(uint8_t addr, uint16_t data)
{
uint8_t txData[3];
txData[0] = addr & 0x7F;
txData[1] = (data >>8) & 0xFF;
txData[2] = data & 0xFF;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET); // Pull CS/SS low
HAL_SPI_Transmit(&hspi1, txData, 3,100);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET); // Pull CS/SS high
}
//Read logic
uint16_t ATM90E26_SPI_Read(uint8_t addr)
{
uint8_t txData= addr | 0x80;
uint8_t rxData[2];
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET); // Pull CS/SS low
HAL_SPI_Transmit(&hspi1, &txData, 1,100);
HAL_SPI_Receive(&hspi1, rxData, 2,100);
// HAL_SPI_TransmitReceive(&hspi1, txData, rxData, 2, 200);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET); // Pull CS/SS high
return (uint16_t)((rxData[0] << 8)| rxData[1]);
}
//ATM90E26 SPI sequence
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-05 8:04 AM
Note that SPI is a bit exchange protocol. For every bit you send you receive a bit. So, given the "SPI sequence" you show you must transmit 3 bytes in order to properly set the register address and transfer the 2 data bytes (for either a read or write operation). You must use a 3-byte HAL_SPI_TransmitReceive() for the register read operation.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-24 5:09 AM
Try enabling the SPI unit before selecting the slave