OC toggle and DMA problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-06-04 7:40 AM
Posted on June 04, 2015 at 16:40
I'm trying to connect the output Compare together with the DMA controller for my STM32F3 discovery board.
But I have a strange problem, it seems like the DMA controller is only copying one byte from the memory to the compare registerDMA disabledCCR2 register100tick => 5.6us200tick =>11.3us300tick=>17.2us400tick=>22.3usbut when using the DMA it seems to only copy one byte from the memory to the CCR2 register100tick => 5.6us200tick => 11.3us300tick => 2.5us = 0x12C, 0x2C => 44 * 5.6/100 = 2.5us400tick => 8.1us = 0x190, 0x90 = >144 * 5.6/100 = 8.1usI've tried to setup the DMA in both half_word and word but still get the same results.Any idea what the problem could be?[code]#define PULSE_LENGTH 0xFFFFuint16_t OC_1_arr[4];void initDebugPort_PE12(void){ GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOE, &GPIO_InitStructure);}void initICport(void){ TIM_ICInitTypeDef TIM_ICInitStructure; TIM_ICStructInit(&TIM_ICInitStructure); TIM_ICInitStructure.TIM_Channel = TIM_Channel_1; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0; TIM_ICInit(TIM8, &TIM_ICInitStructure);}void initOCports_PC7_PC8_PC9(void){ GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6| GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_4); GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_4); GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_4); GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_4);}void initTimer8(void){ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM8, ENABLE); uint16_t PrescalerValue = (uint16_t) ((SystemCoreClock ) / CLOCK_FREQYENCY) - 1; /* Time base configuration */ TIM_TimeBaseStructInit(& TIM_TimeBaseStructure); TIM_TimeBaseStructure.TIM_Period = 0xFFFF; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM8, &TIM_TimeBaseStructure); TIM_SelectOnePulseMode(TIM8, TIM_OPMode_Single); TIM_SelectInputTrigger(TIM8, TIM_TS_TI1FP1); //connect timer8 to trigger on channel 1 TIM_SelectSlaveMode(TIM8, TIM_SlaveMode_Combined_ResetTrigger); TIM_CtrlPWMOutputs(TIM8,ENABLE); TIM_Cmd(TIM8, ENABLE);}void initPA0_and_PA1_As_PWM(void){ TIM_OCInitTypeDef TIM_OCInitStructure; TIM_OCStructInit(&TIM_OCInitStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle; TIM_OCInitStructure.TIM_Pulse = 100; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC2Init(TIM8,&TIM_OCInitStructure ); TIM_OCInitStructure.TIM_Pulse = 300; TIM_OC3Init(TIM8,&TIM_OCInitStructure ); TIM_OCInitStructure.TIM_Pulse = 0x30; TIM_OC4Init(TIM8,&TIM_OCInitStructure ); TIM_OC1PreloadConfig(TIM8, TIM_OCPreload_Disable); TIM_DMACmd(TIM8, TIM_DMA_CC2, ENABLE); // connect timer8 to AF pin}void setupDMA(void){ DMA_InitTypeDef DMA_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA2, ENABLE); DMA_DeInit(DMA1_Channel1); DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_BufferSize = 2; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)OC_1_arr; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&(TIM8->CCR2); //ch2 DMA_InitStructure.DMA_MemoryDataSize = DMA_PeripheralDataSize_HalfWord; //16bit DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_Init(DMA2_Channel5,&DMA_InitStructure); DMA_Cmd(DMA2_Channel5, ENABLE);}void TIM8_Configuration(void){ OC_1_arr[0] = 400; OC_1_arr[1] = 54;// OC_1_arr[2] = 0x120;// OC_1_arr[3] = 0x400; initDebugPort_PE12(); initOCports_PC7_PC8_PC9(); initICport(); initTimer8(); setupDMA(); initPA0_and_PA1_As_PWM();}[\code]
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-06-04 7:56 AM
Posted on June 04, 2015 at 16:56
Might want it to advance
DMA_InitStructure.DMA_MemoryInc
= DMA_MemoryInc_Disable;
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..