2016-03-04 2:47 PM
Hi, i wrote a simple program in Keil uVision to test the HAL SPI driver
The logic analyzer shows that there is clock activity as expected but the MOSI ouput stay low all time even with pull-up enabled (see attached screenshot) Surely i made some mistake somewhere. Here is the listing. Can you help ?#define USE_HAL_DRIVER
#include <stm32f4xx.h>int main () { uint8_t byte; SPI_HandleTypeDef hspi; GPIO_InitTypeDef GPIO_InitTypeDefStruct; __GPIOA_CLK_ENABLE(); __SPI1_CLK_ENABLE(); hspi.Instance = SPI1; hspi.Init.Mode=SPI_MODE_MASTER; hspi.Init.Direction=SPI_DIRECTION_2LINES; hspi.Init.DataSize=SPI_DATASIZE_8BIT; hspi.Init.CLKPolarity=SPI_POLARITY_HIGH; hspi.Init.CLKPhase=SPI_PHASE_2EDGE; hspi.Init.NSS=SPI_NSS_SOFT; hspi.Init.BaudRatePrescaler=SPI_BAUDRATEPRESCALER_16; hspi.Init.FirstBit=SPI_FIRSTBIT_MSB; hspi.Init.TIMode=SPI_TIMODE_DISABLED; hspi.Init.CRCCalculation=SPI_CRCCALCULATION_DISABLED; hspi.Init.CRCPolynomial=0; HAL_SPI_MspInit(&hspi); HAL_SPI_Init(&hspi); GPIO_InitTypeDefStruct.Pin = GPIO_PIN_5 | GPIO_PIN_7 | GPIO_PIN_6; GPIO_InitTypeDefStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitTypeDefStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitTypeDefStruct.Pull = GPIO_PULLUP; GPIO_InitTypeDefStruct.Alternate = GPIO_AF5_SPI1; HAL_GPIO_Init(GPIOA, &GPIO_InitTypeDefStruct); GPIO_InitTypeDefStruct.Pin = GPIO_PIN_4; GPIO_InitTypeDefStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitTypeDefStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitTypeDefStruct.Pull = GPIO_PULLUP; HAL_GPIO_Init(GPIOA, &GPIO_InitTypeDefStruct); byte = 0xAA; // data to be transmitted 0b10101010 while(1) { HAL_GPIO_WritePin(GPIOA,GPIO_PIN_4,GPIO_PIN_RESET); // assert slave select low HAL_SPI_Transmit(&hspi,&byte,1,4); HAL_GPIO_WritePin(GPIOA,GPIO_PIN_4,GPIO_PIN_SET); // assert slave select high }}