2018-10-18 7:25 AM
Hello,
One specification of my system is the long live of my peripheral (Nucleo-L152RE+ IDB05A1). The most time, my peripheral is in advertising mode. I know that as soon as IDB05A1 advertising I can put µc in standby, the IDB05A1 will work autonomously and continue to advertise. If the IDB05A1 find a central it will wake up the microcontroller.
1. I tried to enter low power modes with following pre-built functions:
HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI );
HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFE );
HAL_PWR_EnterSTANDBYMode();
The Microcontroller reach the low power mode but the current is around 1mA which is far too much. In these modes I couldn't wake up the microcontroller.
2. On the web I found following function. With it I had a similar current consumption but the microcontroller is able to be wake up:
void EnterStandbyMode(void)
{
/* Wait that user release the User push-button */
/* Disable all used wakeup sources */
//LL_PWR_DisableWakeUpPin(LL_PWR_WAKEUP_PIN1);
CLEAR_BIT(PWR->CSR, PWR_CSR_EWUP1);
/* Clear all wake up Flag */
//LL_PWR_ClearFlag_WU();
SET_BIT(PWR->CR, PWR_CR_CWUF);
/* Enable wakeup pin */
//LL_PWR_EnableWakeUpPin(LL_PWR_WAKEUP_PIN1);
SET_BIT(PWR->CSR, PWR_CSR_EWUP1);
/* Enable ultra low power mode */
//LL_PWR_EnableUltraLowPower();
SET_BIT(PWR->CR, PWR_CR_ULP);
/** Request to enter STANDBY mode
* Following procedure describe in STM32L1xx Reference Manual
* See PWR part, section Low-power modes, Standby mode
*/
/* Set STANDBY mode when CPU enters deepsleep */
//LL_PWR_SetPowerMode(LL_PWR_MODE_STANDBY);
MODIFY_REG(PWR->CR, PWR_CR_PDDS, PWR_CR_PDDS);
/* Set SLEEPDEEP bit of Cortex System Control Register */
//LL_LPM_EnableDeepSleep();
SET_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SLEEPDEEP_Msk));
/* This option is used to ensure that store operations are completed */
#if defined ( __CC_ARM)
__force_stores();
#endif
/* Request Wait For Interrupt */
__WFI();
}
3. After the wake up the microcontroller restarts. I know which interrupt is incoming but it's incoming a lot of times so I can't find a fitting logic which secure that the microcontroller is not getting in low power mode again.
At the moment when a device want connect to my microcontroller it is in ... standby -> wake up -> standby -> wake up -> stanby...
By the way I work with STM32CubeMX and SW4STM32.
I hope you can help me with the current consumption problem and the logic. If you have any ideas about this issues, feel free to share your thoughts
Best regards,
Tobias