2018-02-06 9:47 AM
I am seeing a problem with couple of my Nucleo L073RZ REV C boards which starts to heat up when powered using VIN i.e 12V supply. The boards are working fine, but I can feel the temperature increase if I touch the backside of R29/R30 resistors.
If the board is powered through USB or even if USB cable is connected (powered using VIN) I don't see the temperature rise. Anyone know the reason for the same.
Thanks
Hemanth
2018-02-06 11:11 PM
I would try reducing the input voltage, say, to 9V or less.
Most cheap 'wall warts' have a considerably higher output voltage at low load conditions.
2018-02-06 11:18 PM
If you didn't realize it - the voltage regulator at Vin (LD1117S50) is of the linear type.
It converts (Vin - 5.0V) * Iout into heat.