2018-02-06 11:21 PM
Hi All,
I had found a problem with STM32L486, That I connect this pin with 100K pull up to 3V3 and a 0.1uF cap to GND. It won't work when I drag&drop through SWDIO/SWDCLK .hex files in to it. But if I connect this 'Reset' pin just with 0.1uF cap to GND, or connect this pin with 10K pull up to 3V3 and 0.1uF cap to GND. it works fine(can drag&drop .hex file in to it)
Any one have ideas about this?
2018-02-07 12:36 AM
Hello Kevin,
There is no need to connect external pull-up resistor to NRST pin of STM32L4 MCU. Pull-up resistor is already embedded in internal reset circuitry (it is called Rpu). Please find below a relevant block diagram. Rpu has typically value 40kOhm.
It could be that external pull-up 100kOhm is too strong and together with internal pull-up they don't allow reset signal to reach a threshod needed to reset the MCU.
External pull-up
10kOhm is normally ok, but again please note, that this is not mandatory. Only 100nF capacitor between NRST and ground is needed.
I would suggest either to use external pull-up
10kOhm or to remove completely external pull-up resistor.
Regards
Szymon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.