cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-H743ZI2, Unknown USB Device

Sheraz2568
Associate II

image_2023_09_26T13_36_43_009Z.png

Hello,

I'm attempting to set up the CN13 USB port as a Virtual COM Port (VCP) for transferring data to LabVIEW. Unfortunately, I'm encountering an error message that reads "Unknown USB Device (Device Descriptor Request Failed)." I've already installed the relevant drivers, but the issue persists.

 

NOTE: I am trying to USB_FS for high-speed data transferring to LabVIEW as alternative for UART. 

 

image_2023_09_26T13_36_43_009Z.png

4 REPLIES 4
Issamos
Lead II

Hello @Sheraz2568 

I suggest you to click on the unknown USB device and update the driver. That may solve the issue.

Best regards.

II 

Pavel A.
Evangelist III

This means that Windows cannot read the required USB device descriptors (it even says so in plain text: "device descriptors request failed"). Debug your firmware, find which request fails. 

Note: fumbling with drivers on the Windows side won't help until the device can be recognized correctly.

FBL
ST Employee

Hello @Sheraz2568 

Did you try to access DFU mode? If not, check this post.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


I'm out of offce with limited access to my emails.
Happy New Year!

Hello @Issamos 

Yes! Already did that before posting here, but it didn't work out. 

Thank you