cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F042K6 + Keil? How?

sseveelavanan9
Associate II
Posted on April 27, 2016 at 18:30

Hi gang,

How do I set up Keil with this new dev board, including the ST-Link/V2-1?

Cant see this board in the

http://https://www.keil.com/boards2/

 (as I guess is quite new). But actual

http://https://www.keil.com/dd2/st/stm32f042k6/

is in the

http://https://www.keil.com/dd2/

.

I've installed the 'Device Family Pack', and so can now see the STM32F042K6 from within the 'Device Database'.

Cheers

#nucleo #keil
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Nesrine M_O
Lead II
Posted on April 28, 2016 at 12:59

Hi chendy,

Try to use the Pack Installer to install the Software Pack, or try to download and install the pack directly from this

http://www.keil.com/dd2/st/stm32f042k6/

.

-Syrine –

sseveelavanan9
Associate II
Posted on April 29, 2016 at 13:14

I have done so, but what next to get a pin toggling etc?

Are there any guides for setting up a new project for a board that is currently unsupported (despite it being sold to me!)?

thanks

Nesrine M_O
Lead II
Posted on April 29, 2016 at 15:23

Hi chendy,

STM32Cube_FW_F0_V1.5.0\Projects\STM32F042K6-Nucleo\Examples

this directory contains a set of examples based on STM32F042K6-Nucleo board, it will be very helpful as staring to develop your own application.

-Syrine –

sseveelavanan9
Associate II
Posted on May 10, 2016 at 16:07

Are there any examples for USB Serial?

Posted on May 10, 2016 at 17:46

Are there any examples for USB Serial?

Using the VCP provided by the Nucleo board, or running natively on the F042K6 ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..