2016-04-21 5:51 AM
Heloo,
I Get some Randon Value when i call for data receive. I kindly request you to provide me soultion for my code.SPI config in Mainis declared as :void MX_SPI1_Init(void){ hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_2EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 7; HAL_SPI_Init(&hspi1);}I am trying to receive and transmit value . Is this the way you transmit and receive a value using SPI communication.void ADS1220SendByte(uint8_t Byte){ uint8_t *dummy; /* Call SPI read generic function */ if(HAL_SPI_Transmit(&hspi1, (uint *)Byte, 1,5000) != HAL_OK) { set_ERROR(); } // if(HAL_SPI_Receive(&hspi1, dummy, 1,5000) != HAL_OK)// {// set_ERROR();// } }unsigned char ADS1220ReceiveByte(void){ unsigned char *Result; /* Call SPI read generic function */// if(HAL_SPI_Transmit(&hspi1, (uint8_t *)0xFF, 1,5000) != HAL_OK)// {// set_ERROR();// } if(HAL_SPI_Receive(&hspi1, Result, 1, 5000) != HAL_OK) { set_ERROR(); } return *Result;} #stm32l053 #stm32f4 #nucleo #nucleo #discovery #spi #spi #!stm32 #device2016-04-21 7:11 AM
Hi malladi.sandeep.001,
I recommend you to have a look to SPI examples under the STM32L0 cube firmware package, it may be helpful :STM32Cube_FW_L0_V1.5.0\Projects\STM32L053R8-Nucleo\Examples\SPI-Syrine-2016-04-25 1:28 AM
Hello Syrine,
Thanks for the reply but my problem is i am able to communicate with the slave device using STM32-Nucleo L053R8 board but when i read a particular register by call SPI read and Write i get differnt values if i tell SPI to read a particular rigester value it gives some value as 0x00000008 but while writing in to particular register the value is 0x00000000 i am unable to identify the problem could you please help me out. I here by send my code that i had implemented.void ADS1220Config(void){ //ADS1220ReadRegister(ADS1220_0_REGISTER, 0x01, &Temp); // clear prev value; // Temp &= 0x0f; Temp1 |= ADS1220_MUX_0_G; // write the register value containing the new value back to the ADS ADS1220WriteRegister(ADS1220_0_REGISTER, 0x01, &Temp1); //ADS1220ReadRegister(ADS1220_1_REGISTER, 0x01, &Temp); // clear prev DataRate code; //Temp &= 0x0f; Temp2 |= (ADS1220_DR_20 + ADS1220_CC); // Set default start mode to 600sps and continuous conversions // write the register value containing the new value back to the ADS ADS1220WriteRegister(ADS1220_1_REGISTER, 0x01, &Temp2); }my spi Transmit and receive functions are this way void ADS1220SendByte(uint8_t Byte){ if(HAL_SPI_Transmit_IT(&hspi1,&Byte, sizeof(Byte))!= HAL_OK) { /* Transfer error in transmission process */ set_ERROR(); } while (HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY) { } }unsigned char ADS1220ReceiveByte(void){ uint8_t Result; if(HAL_SPI_Receive_IT(&hspi1,&Result, sizeof(Result))!= HAL_OK) { set_ERROR(); } while (HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY) { } return Result;}Can you please look in to the code. Thanks