cancel
Showing results for 
Search instead for 
Did you mean: 

Nucelo F207ZG USB CDC Example code

Manikandan K
Associate III
Posted on March 22, 2017 at 08:50

Hi, I'm using Nucleo F207ZG board and i did my testing of GPIO using STM32CubeMx(HAL lib) with Eclipse IDE on Ubuntu 04, Now i want to use the USB as Communication Device Class (CDC) but i'm not familiar with usb so is there any example coding for tranfer the data from/to Nucleo board/PC

Note: this post was migrated and contained many threaded conversations, some content may be missing.
20 REPLIES 20
Manikandan K
Associate III
Posted on June 09, 2017 at 15:26

Hi ,

USB receive class file only receive up to 18 byte properly (tested in the GTK Term tool) ,  I'm using receiving size as 64 only .

Pls Any suggestion

K.Manikandan