2018-03-21 06:16 AM
Hi awesome people,
I am new to MCU programming and I am doing an image processing project in pattern recognition. I am using STM3241G-EVAL development kit. I am not able to boot up my kit on my laptop(Windows 10). I connected the power cable and the usb cable but still its not booting up
2018-03-21 08:33 AM
Is there a jumper to select the power source?
Which USB? ST-LINK?
Is it running code that would support connectivity as a USB HS/FS device?
Does it power from 5V DC wall-wart supply?
2018-03-21 12:26 PM
Ok, but what does '
not booting up
' mean to you?Is this a new board, or has someone else used it already? Loading other examples will wipe the demo app.
Have you connected to the ST-LINK USB connector? CN21
Have you installed the drivers?
Have you build and downloaded any of the example applications?
Are you working with a local ST office or FAE?
2018-03-26 04:18 AM
hey,
thanks for your help. I tried changing the jumper and it worked. thanks a lot