2013-02-27 12:28 AM
Hi
I am trying to command a Pololu Maestro device from my STM32 device. The Pololu requires a non-inverted TTL signal for commands. I can send out the command through an attached UART board to a hyperterminal session on my PC but as I understand the PL 2303 on that addon board inverts the signal. I actually wanted to use the SW-attached UART-Pin as Tx signal. I tried to find a setting for the UART or Pin to be non-inverting but could not see anything like that. Can I define a Pin to be always in the inverted state of another Pin? Juerg #uart2016-02-12 04:40 AM
(void)EXTI->PR;
That should be enough to cope with the behavior I explained. If you did not solve the issue with the ''while'' loop (never write such an unlimited while loop inside an interrupt handler), the ground reason should be something else.