2016-08-08 1:39 PM
Hi, I just set up DAC output on the STM32F303 Discovery Board and I'm noticing a lot of wideband noise on the output (about .5 volts peak to peak), even when I set it to a constant value within my program. Is there something in the way I'm am setting up DAC output that might be causing this? I based the output configuration off of the DMA_RAM_DAC peripheral example project.
Here is my code for setting up DAC output, please let me know if you see anything: int main(void){ /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f30x.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f30x.c file */ DMA_Config(); DAC_Config(); TIM_Config(); while (1) { DAC1Output = 4095; }}/** * @brief Configures the TIM2 * @param None * @retval None */static void TIM_Config(void){ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; /* TIM2 Periph clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); /* Time base configuration */ TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); TIM_TimeBaseStructure.TIM_Period = 0xFF;//0xFF; TIM_TimeBaseStructure.TIM_Prescaler = 0x0; TIM_TimeBaseStructure.TIM_ClockDivision = 0x0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); /* TIM2 TRGO selection: update event is selected as trigger for DAC */ TIM_SelectOutputTrigger(TIM2, TIM_TRGOSource_Update); /* TIM2 enable counter */ TIM_Cmd(TIM2, ENABLE);}/** * @brief Configures DAC channel 1 and channel 2 * @param None * @retval None */static void DAC_Config(void){ DAC_InitTypeDef DAC_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable GPIOA Periph clock --------------------------------------*/ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /* Configure PA.04 (DAC1_OUT1), PA.05 (DAC1_OUT2) as analog */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); /* DAC Periph clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_DAC, ENABLE); /* Fill DAC InitStructure */ DAC_InitStructure.DAC_Trigger = DAC_Trigger_T2_TRGO; DAC_InitStructure.DAC_WaveGeneration = DAC_WaveGeneration_None; //DAC_InitStructure.DAC_LFSRUnmask_TriangleAmplitude = DAC_TriangleAmplitude_4095; DAC_InitStructure.DAC_OutputBuffer = DAC_OutputBuffer_Disable; /* DAC channel1 Configuration */ DAC_Init(DAC_Channel_1, &DAC_InitStructure); /* DAC channel2 Configuration */ DAC_Init(DAC_Channel_2, &DAC_InitStructure); /* Enable DAC Channel1: Once the DAC channel1 is enabled, PA.04 is automatically connected to the DAC converter. */ DAC_Cmd(DAC_Channel_1, ENABLE); /* Enable DAC Channel2: Once the DAC channel2 is enabled, PA.05 is automatically connected to the DAC converter. */ DAC_Cmd(DAC_Channel_2, ENABLE); /* Enable DMA for DAC Channel1 */ DAC_DMACmd(DAC_Channel_1, ENABLE);}/** * @brief Configures DMA2 channel3 * @param None * @retval None */static void DMA_Config(void){ DMA_InitTypeDef DMA_InitStructure; /* Enable DMA2 clock -------------------------------------------------------*/ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA2, ENABLE); DMA_DeInit(DMA2_Channel3); DMA_InitStructure.DMA_PeripheralBaseAddr = DAC_DHR12RD_Address; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&DAC1Output; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_BufferSize = 1; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA2_Channel3, &DMA_InitStructure); /* Enable DMA2 Channel3 */ DMA_Cmd(DMA2_Channel3, ENABLE);} #stm32 #dac #noise #stm32f3032016-08-16 9:05 AM
Hi ,
Be careful to these points :+ Check if thePeripheralBaseAddr ''DAC_DHR12RD_Address;'' is correct . T think the corret one is ''DAC_DHR12R2_Address;''
+ Check the wave generation parameters which is set to none . I think it should be chaged to ''DAC_WaveGeneration_Triangle''-Hannibal-