2014-06-30 1:32 AM
Hi,
On our board which contains stm32f105R8, I can see no usart1 activity. I'ved used the supplied ST printf example to configure usart1. Our board has an external 8MHz crystal and I've seen it mentioned that the CL series expects an external 25Mhz crystal by default, so that may be the issue. I have set the XTAL clock value to be 8MHz in uVision4 tools hoping that would solve our problem but no luck. Does anyone have the correct settings for stm32f10x.h in order to use the external 8 Mhz crystal to generate a system clock of 48 Mhz? Thank you Bob2014-07-07 12:49 AM
Hi Clive,
In order to get the uart working, I had to remove the SysClock_Config line. If I leave this line inserted, the usart will hang after printing 10 characters. However I need SysClock running in order to generate a delay. The Vector table contains the proper SysTick_Handler address. The clocks are up and stable at 48 MHz. I can see then on MCO pin. Any ideas Clive why no delay occurs or why it kills the usart? Is it an exception that I'm not handlind or is SysTick even confugured properly? Thanks Bob int main(void) { RCC_ClocksTypeDef RCC_Clocks; // Enable SYSCFG clock SetSysClockTo48() ; /* SysTick end of count event each 1ms */ RCC_GetClocksFreq(&RCC_Clocks); /* SysTick_Config(RCC_Clocks.HCLK_Frequency / 1000); */ USART works when commented */ /* Switch ON all clocks to the ports */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); Usart1Init(); // Console /*Delay(1000); * /*Code will hang at this line if SysTick Enabled */ printf(''\n\rHello World\n\r''); } The SysTick handler is as per supplied example. /** * @brief This function handles SysTick Handler. * @param None * @retval None */ void SysTick_Handler(void) { TimingDelay_Decrement(); }/**
* @brief Inserts a delay time. * @param nTime: specifies the delay time length, in milliseconds. * @retval None */ void Delay(__IO uint32_t nTime) { TimingDelay = nTime;while(TimingDelay != 0);
}/**
* @brief Decrements the TimingDelay variable. * @param None * @retval None */ void TimingDelay_Decrement(void) { if (TimingDelay != 0x00) { TimingDelay--; } }2014-07-07 9:32 AM
Not sure what's going on here. There are later version of Keil uv 4.7x that had some reported issues with volatile variables.
The clocking settings within v3.5.0 of the F1 firmware library are typically handled in SystemInit(), which is called prior to main() I wouldn't permit main() to exit. In the debugger where does the code appear to be stuck or end up?2014-07-07 10:09 AM
I might do it like this:
/*
STM32F107VC - USART1 + SysTick demo - sourcer32@gmail.com
STM32F10x_StdPeriph_Lib_V3.5.0
Startup : startup_stm32f10x_cl.s
System : system_stm32f10x.c
Project defines : USE_STDPERIPH_DRIVER, STM32F10X_CL
HSE_VALUE must reflect external crystal
*/
#include ''stm32f10x.h''
#include <
stdio.h
>
#include <
stdlib.h
>
//****************************************************************************
void USART1_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable GPIO and USART1 clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_USART1, ENABLE);
/* Configure USART Tx as alternate function push-pull */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Configure USART Rx as input floating */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* USARTx configured as follow:
- BaudRate = 115200 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
/* USART configuration */
USART_Init(USART1, &USART_InitStructure);
/* Enable USART */
USART_Cmd(USART1, ENABLE);
}
//****************************************************************************
volatile int SystemTick = 0;
#define TICK_RATE 1 // in milliseconds
void SysTick_Handler(void)
{
// Free running millisecond counter for timeouts
SystemTick += TICK_RATE; // 1 ms tick count
}
//****************************************************************************
int Sleep(int Delay)
{
int Start, Current;
Start = SystemTick;
do
{
// __WFI(); // Wait for interrupt - kills debugger if low power kicks here
Current = SystemTick;
}
while((Current - Start) <
Delay
);
return(Current - Start); // Estimate of time past
}
//****************************************************************************
int main(void)
{
RCC_ClocksTypeDef RCC_Clocks;
/*!< At this stage the microcontroller clock setting is already configured,
this is done through SystemInit() function which is called from startup
file (startup_stm32f10x_xx.s) before to branch to application main.
To reconfigure the default setting of SystemInit() function, refer to
system_stm32f10x.c file
*/
RCC_GetClocksFreq(&RCC_Clocks);
if (SysTick_Config(RCC_Clocks.SYSCLK_Frequency / 1000))
{
/* Capture error */
while (1);
}
/* Add your application code here
*/
printf(''Hello World!
'');
while(1)
{
Sleep(5000);
puts(''HELP!'');
}
while(1); /* Infinite loop */
}
//****************************************************************************
// Hosting of stdio functionality through USART1
//****************************************************************************
#include <rt_misc.h>
#pragma import(__use_no_semihosting_swi)
struct __FILE { int handle; /* Add whatever you need here */ };
FILE __stdout;
FILE __stdin;
int fputc(int ch, FILE *f)
{
while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);
USART_SendData(USART1, ch);
return(ch);
}
int fgetc(FILE *f)
{
char ch;
while(USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET);
ch = USART_ReceiveData(USART1);
return((int)ch);
}
int ferror(FILE *f)
{
/* Your implementation of ferror */
return EOF;
}
void _ttywrch(int ch)
{
while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);
USART_SendData(USART1, ch);
}
void _sys_exit(int return_code)
{
label: goto label; /* endless loop */
}
//****************************************************************************
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d
'', file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif
//****************************************************************************
2014-07-07 3:45 PM
Thanks Clive,
I'll try this tomorrow. Regards Bob2014-07-08 4:55 PM
Hi Clive,
I tried this and it was the same..it didn't work. I checked the SysTick registers after configuration and I got the following...(in decimal) SysTick Control Register = 7 SysTick Reload Value = 47999 SysTick Current value (starts at 47998 and updates contantly when the app is run. However the count is random and I can make no sense of whether it is meant to be up or down) SysTick Calibration Value = 1073750824 SystemTick never increments when app is running so the delay never occurs. I'm lost at this stage. The SysTick Handler is at the correct location in the vector table, so I really don't know what could be causing this. Regards Bob2014-07-08 6:04 PM
Not got much idea about what's going on with your system.
I'd have to take a look at the schematic, and a complete zipped up project with output files.2014-07-09 3:56 AM
CLKSOURCE
0 = external reference clock.
1 = core clock.
If no reference clock is provided, it is held at 1 and so gives the same time as the core clock. The core clock must be at least 2.5 times faster than the reference clock. If it is not, the count values are Unpredictable.
2014-07-09 5:43 AM
Probably not, the external SYSTICK source on the STM32 parts is HCLK/8
2014-07-09 3:23 PM
Yep you're correct Clive no difference. Only other thing I can think off is vector table address mismatch, but they look to be ok. SysTick Handler Address is specified as 0x8000420D but the map file states that its address is 0x0800420c. I think this is OK though. The contents of SCB->VTOR are 0x08003000. Does that seem correct?
Bob2014-07-09 4:52 PM
The ODD addressing of the routines in memory reflects that they are 16-bit Thumb code rather than 32-bit ARM.
The +0x3000 offset for the vector table suggests you have some other boot loader app, which might well be complicating the discussion here. If you are building the project with a base of 0x08000000 this could well be a problem.