2013-12-23 11:19 PM
As m a newbie to STM32 need help on following:
I am using ST-Link from STM32F0 discovery board (jumpers removed as provided in PDF), for connection with STM32F373xx .Connections:SWD(on F0) PINS ON MCU(STM32F373CB)1 Connected to VDD_1(pin no 48)2 SWCLK (pin no 37)3 GND(pin no 47)4 SWDIO (pin no 34)5 NRSTwhile VDD_1, VDD_2 and VDDA are connected to 3V of F0 BOARD.It shows ''No Target Connected''.(Settings of SW in the IDE are done and selected STLINK Debugger) #no-target-coonected-stm32f373xx