2008-11-13 10:15 PM
no output of USART with STM32-H103 board
2011-05-17 3:52 AM
Hallo everybody,
I am new with the Cortex M3 and have some problems using the UART. I can´t see any output on Windows Terminal. I use CrossStudio for ARM with Olimex ARM-USB-OCD and this is the source codes : void RCC_Configuration(void) { RCC_DeInit(); // 2. Enable ext. high frequency OSC RCC_HSEConfig(RCC_HSE_ON); // wait until the HSE is ready while(RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET); // 3. Init PLL RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_9); // 72MHz RCC_PLLCmd(ENABLE); // wait until the PLL is ready while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET); // 4. Set system clock divders /* RCC_USBCLKConfig(RCC_USBCLKSource_PLLCLK_1Div5); */ RCC_HCLKConfig(RCC_SYSCLK_Div1); // AHB Clock = 72 MHz RCC_PCLK2Config(RCC_HCLK_Div1); RCC_ADCCLKConfig(RCC_PCLK2_Div8); // ADC Clock = 8 MHz RCC_PCLK1Config(RCC_HCLK_Div2); // Flash 1 wait state *(vu32 *)0x40022000 = 0x12; // 5. Clock system from PLL RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); while(RCC_GetSYSCLKSource() != 0x08) { } RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO | RCC_APB2Periph_ADC1 |RCC_APB2Periph_AFIO | RCC_APB2Periph_USART1, ENABLE); } int main (void) { #ifdef DEBUG debug(); #endif /* System clocks configuration ---------------------------------------------*/ RCC_Configuration(); // Configure PA.9 (USARTT1_TX) as output Open Drain Output Alternate-Function GPIO_ResetBits(GPIOA,GPIO_Pin_9); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_9; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_OD; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStruct); USART_Configuration(); USART_Cmd(USART1, ENABLE); while(1) { USART_SendData(USART1, 0xaa); while(!USART_GetFlagStatus(USART1, USART_FLAG_TXE)) { } while(!USART_GetFlagStatus(USART1, USART_FLAG_TC)) { } } } /*******************************************************************************/ void USART_Configuration(void) { USART_InitTypeDef USART_InitStruct; /* Configure -------------------------*/ USART_InitStruct.USART_BaudRate = 9600; /* 9600 Baud */ USART_InitStruct.USART_WordLength = USART_WordLength_8b; USART_InitStruct.USART_StopBits = USART_StopBits_1; USART_InitStruct.USART_Parity = USART_Parity_No ; USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStruct.USART_Mode = USART_Mode_Tx; /* USART_InitStruct.USART_Clock = USART_Clock_Enable; USART_InitStruct.USART_CPOL = USART_CPOL_Low; USART_InitStruct.USART_CPHA = USART_CPHA_1Edge; USART_InitStruct.USART_LastBit = USART_LastBit_Disable; */ USART_Init(USART1, &USART_InitStruct); } I have tested the output of UART Tx Pin with oscilloscope but there is output signal. Before i have already test program loading by the simple ''blinky'' program and it´s ok. I really have no idea. Could someone help me ? thank u