cancel
Showing results for 
Search instead for 
Did you mean: 

RTC and TIMER2 and SYSTICK

hervett
Associate II
Posted on November 19, 2008 at 04:16

RTC and TIMER2 and SYSTICK

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
hervett
Associate II
Posted on May 17, 2011 at 12:52

Hello everybody !!On my program I want to have a signal of 400 Khz with my timer2 in PWM mode and have the RTC for the clock, on. RTC work without the Timer2, Timer2 work without RTC, but when I try to have them at the same time it doesn't work and the systick too. I try all the possibilities of the priority. I tried to do like the demo program of the STM32F10B because there is RTC, systick and TimeR2 together. I tried on TIMER3, the same. And today, still doesn't work. I think I have try everything...Maybe someone had the same problem.... :-[ :-[ :-[ :-[ :-[ .......

I will accept help from anybody.

Thanks a lot !

franco2399
Associate II
Posted on May 17, 2011 at 12:52

Hy Hervett,

I using STM32F103RE with ST320F10x-E Eval board, RTC and Timer1 togher without problems:

-Timer 1 from HSE 8Mhz-> 48MHz with pwm function at 20KHz frequency

-RTC from LSE 32KHz for wakeup during stop mode

The systick is set at 32ms.

by

franco2399
Associate II
Posted on May 17, 2011 at 12:52

Hy Hervett,

I using STM32F103RE with ST320F10x-E Eval board, RTC and Timer1 togher without problems:

-Timer 1 from HSE 8Mhz-> 48MHz with pwm function at 20KHz frequency

-RTC from LSE 32KHz for wakeup during stop mode

The systick is set at 32ms.

by

hervett
Associate II
Posted on May 17, 2011 at 12:52

It's OK now, My program work with my TIMER2 in PWM, my RTC and the Systick, but still don't work wth my Timer2in Output compare toggle mode. So I will keep the PWM for my 400 kHz.

I havn't do something special, it is just the difference between PWM ans Output compare toggle mode.

Bye