cancel
Showing results for 
Search instead for 
Did you mean: 

No I2C Clock signal after Restart Condition

uli stone
Associate II

Hello,

I raised this problem in another topic I posted, but it is with another title and I'm not sure I will get there the help (title might be missleading).

I have the problem after sending Slave Address and Register Address and creating a start condition I don't get any clock signal from the STM32F4 microcontroller.

Hoch can I solve this?

Thank you0690X000006DUzQQAW.png

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
uli stone
Associate II

Thanks @Danish​ for the info.

Changed in Stop to I2C_SR2_MSL and removed the for-loop. Result is no clock pulses after the Stop-Start-Condition.

I think it's now about the sensor not about the microcontroller, the StdLib might somehow introduce a longer time for stop-start.

For now I would not mind to leave the for loop there, I want to get the interface now working. I have spend a lot of time and not able to read the reply of the sensor.

How can I provide a clock impulse for the sensor after the second address? Where should I check and reset which register?

thank you very much

Uli

Mon2
Senior III

Hi @uli stone​ . Sorry to jump in the middle of this dialog but is it important for you to use a step-by-step I2C handshake with your project? For example, why not apply the very powerful DMA feature of the I2C port using one of the working examples from CubeMX, etc. ? Most of the time, such examples can be working in a few minutes. The STM32F4 is very powerful and offer interrupt / DMA use to quickly send / receive data over I2C bus. You can also follow the examples to build an I2C slave using one of the kits.

Danish1
Lead III

If the I2C peripheral won't do it, then it presumably thinks it has reason not to do it.

Here's where it becomes something of a detective-game. You need to collect all the clues.

What I eventually had to do to sort out my I2C code was - whenever I was about to write to a control register - log the I2C status register(s), the time in microseconds, where I was in my code and what I was just about to do.

Those figures in the reference manual show master-read and master-write, with what events should happen to trigger each next step in your code. Sadly they don't show master-write-restart-read, or what might indicate failure so you can abort without waiting forever.