cancel
Showing results for 
Search instead for 
Did you mean: 

NMI on STM32F103VC

steve23
Associate II
Posted on May 25, 2009 at 17:49

NMI on STM32F103VC

2 REPLIES 2
steve23
Associate II
Posted on May 17, 2011 at 13:12

Hello,

because of safety reasons I need so trigger an NMI via an external line. Is there any way get this working on the STM32F103VC?

I read the reference manual and the datasheet and didn't find anything helpful for this problem (maybe, I did just look for the wrong info).

I appreciate any help.

Thanks and Regards.

Steve

swhite
Associate III
Posted on May 17, 2011 at 13:12

According to Table 36 in section 8.1.2 (and section 6.2.7) of the STM32F103xx Reference manual

''The RCC Clock Security System (CSS) is linked to the NMI vector.''

I don't think you can directly connect the NMI to an external pin :(