cancel
Showing results for 
Search instead for 
Did you mean: 

Need support to use serial monitor in arduino ide or in putty through SWD pins PA13 and PA15 in STM32 Nucleo L152RE Board

ASing.28
Associate II


_legacyfs_online_stmicro_images_0693W00000bj8E4QAI.png 

12 REPLIES 12

SWDIO and SWCLK would facilitate an SWD update method. They would not facilitate a serial port connection, or Arduino Serial Monitor.

You'd perhaps look at using an ST-LINK/V3 pod with a USART.

Or using USB connection of Target MCU and a loader facilitating a CDC Device that appears as a COM Port on the Host PC.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Check if break-off ST-LINK/V2-1 on the NUCLEO board provides USART via a two pin TX/RX Header​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ASing.28
Associate II

Ok!