cancel
Showing results for 
Search instead for 
Did you mean: 

Need suitable External Flash Loader - STM32F423ZHT6 GD25S512MDYIGR

Meenakshi
Associate II

Hi,

I'm creating a project on GUI using an embedded wizard. While I'm trying to flash the code to my STM32F423ZHT6 custom board. It shows an error: failed to erase memory.

I'm using STM32CubeProgrammer and I successfully erased the entire flash. But still it shows the same error. I'm using GD25S512MDYIGR QSPI Flash memory. So I need a suitable flash loader for the STM32CubeProgrammer.

Regards,

Meenakshi.

1 REPLY 1

I can probably construct one, but would need the pin designations for the QSPI interface you have built.

https://github.com/cturvey/stm32extldr/blob/main/README.md

GD25S512MD

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..