cancel
Showing results for 
Search instead for 
Did you mean: 

Need help on External memory loader on STM32H7B0 with W25Q128

Yuvaraj
Associate II

Hi EveryOne,

                  I have made a custom board with STM32H7B0 and  W25Q128 . where W25Q128 has to hold the user application . I hoped that i can change OSPI in STM32H7B0  to a QSPI config and work with W25Q128  ( which will only work with SPI or Qspi) . I can't able to select QSPI config ( which is mentioned as it is already activated ) in Octal SPI parameters . i'm using  firmware version :FW H7 1.12.1 

Yuvaraj_0-1753734104038.png

 

 since this is a personal one i can't change the  W25Q128 to another OSPI supported flash memory  IC. Is there any example or any other way to make   W25Q128 ( changing OSPI to single SPI or using any one SPI communication )  as a external memory to hold user application for  STM32H7B0. 

0 REPLIES 0