cancel
Showing results for 
Search instead for 
Did you mean: 

My NUCLEO L496ZGP stopped working.

MUmer.1
Associate

I was Displaying HSI on Serial Port using Alternate Functions, as soon i enabled the HSI i got the following error messege.

Target no device found

Reason: No device found on target.

Looking Forward for help.

Regards.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andrew Neil
Super User

"Displaying HSI on Serial Port using Alternate Functions"

What do you mean by that?

"as soon i enabled the HSI i got the following error"

Do you mean

  • in the same code, as soon as it reaches the point of enabling HSI?
  • you changed the code?
  • other?

"Target no device found Reason: No device found on target."

Have you checked connections, power supplies, etc?

Did you change the code to go into a sleep mode, and/or disable the debug pins?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.